STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7B3 bricked after flashing!

Hi,I'm trying to program code into custom PCB with STM32H7B3.I was first able to connect to STM32H7B3 (read Device ID etc.), but after flashing, the target cannot be found!ERROR: STM32: Connecting to CPU via connect under reset failed.I created code ...

Tuoman by Senior II
  • 3462 Views
  • 5 replies
  • 0 kudos

What if callback function is interrupted?

On the STM32L0 I have a callback defined based on RTC alarms. In parallel I have a number of external interrupt (EXTIs) . Scenario Callback function is running due to RTC Alarm interrupt. Now EXTI is triggered as well (or visa verse -> EXTI function ...

Different ADC's VREF

Hi all,I am working with the ADC of the STM32G484 microcontroller, and I would need to have two different reference voltages, in order to gain resolution.I can't find anything about this in the datasheet, so it leads me to think that it is not possib...

JTánt.1 by Associate II
  • 1009 Views
  • 1 replies
  • 0 kudos

Stm32f072 external interrupts more than one

In my project am using A mcu , and wanted to use pA0 and Pc13 as two interrupt.​But interrupt for pA0 is not coming and Pc13 is coming.​Please help to know the cause.​Rohit+91-8141616356​

RKade.1 by Associate III
  • 2603 Views
  • 9 replies
  • 1 kudos

How do I get my flash programmer to reset an STM32G070 after programming it, so that I do not need to cycle power to run the just-download code?

I've tried using IAR and the Segger Flasher to program an STM32G070. However, neither programmer will reset the MCU, so that I do not need to cycle power to run the just-download code? I've seemingly tried every type of Reset. What am I missing?

DBroo.1 by Associate III
  • 3302 Views
  • 3 replies
  • 0 kudos

i use the stm32h750b-dk\demonstrations\toughgfx\mdk-arm\project.uvproj perform assembly, no issue. then perform Download, i increase the ram for alogorithm size, and add MT25L01G_STM32H750B-Disco, erase - > programming - > verify. All ok, no issue.

i use the stm32h750b-dk\demonstrations\toughgfx\mdk-arm\project.uvproj perform assembly, no issue. then perform Download, i increase the ram for alogorithm size, and add MT25L01G_STM32H750B-Disco, erase - > programming - > verify. All OK, no issue. b...

KLau.1 by Associate II
  • 725 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.