STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H753 writing to Flash

Hi , i am using STM32H753 MCU, it has 2 banks of 8 sector each using HAL_FLASH_PROGRAM function , it is not working, can anyone help me with this issue.int data;StartSectorAddress = 0x080E0000eg:(HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, StartSe...

MKS by Associate II
  • 7537 Views
  • 8 replies
  • 0 kudos

data retention

i am using stm32h743zt6 controller, what is meant by data retention in flash memory?where this parameter?how we can calculate this?Thanks,

Tkuma.1 by Associate II
  • 1294 Views
  • 1 replies
  • 0 kudos

Hi, I am new to the STM32. The function SystemCoreClockUpdate() in the library file system_stm32f10x.c extracts the PLL multipl. factor PLLMUL[3:0] from the RCC_CFGR register. Question: why the '+2' here: pllmull = ( pllmull >> 18) + 2;

void SystemCoreClockUpdate (void){  uint32_t tmp = 0, pllmull = 0, pllsource = 0;  /* Get SYSCLK source -------------------------------------------------------*/  tmp = RCC->CFGR & RCC_CFGR_SWS;    switch (tmp)  {    case 0x00:  /* HSI used as system...

Kmax18 by Senior II
  • 2023 Views
  • 2 replies
  • 0 kudos

ADC1 behaving strangely on a STM32L496AGI6.

Hi forum.I have a question regarding the STM32L496G-discovery board. I want ADC1 to sample PC4 located on the on board Arduino connector, take 10 samples for this example and have the DMA xfer these to memory. I have a CubeIde project set up and have...

kvresto by Senior
  • 3424 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.