cancel
Showing results for 
Search instead for 
Did you mean: 

I can jump without problem inside the main memory and boot a second software. Can I do the same thing with the SRAM1? I've copied data from main memory (0x0802000 to SRAM1: 0x20001000), but I can't jump to that address

LFerr
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Which part?

You can run code from RAM at 0x20000000+ typically

You can't jump to 0x20001000, for example, as it is EVEN, and executable THUMB code is referenced at ODD addresses.

The Vector Table contains a list of addresses, and is not inherently executable, the addresses in the list are also absolute so if moved need to be relocated appropriately.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.