cancel
Showing results for 
Search instead for 
Did you mean: 

How can I read all the used ADC channels spread out on all three converters?

Jorgen1
Associate II

I have a configuration where I have 24 single-ended ADC channels distributed on all three ADC channels.

I have not found any example how to read more than one channel.

All channels should be read every 20ms, so there's enough time. But I don't know if it's best to setup three subsequent DMA operations to get a single sample for each channel on each converter, or if regular polling can be done in some kind of optimized way.

This is the way I made it work, but I guess it can be done better.

    sConfig.Rank = ADC_REGULAR_RANK_1;
    sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
    sConfig.SingleDiff = ADC_SINGLE_ENDED;
    sConfig.OffsetNumber = ADC_OFFSET_NONE;
    sConfig.Offset = 0;
    for (int i = 0 ; i < ADC_CHANNEL_COUNT ; i++)
    {
        sConfig.Channel = m_channels[i].channel;
        ASSERT( HAL_ADC_ConfigChannel(m_channels[i].p_handle, &sConfig) == HAL_OK );
 
        ASSERT( HAL_ADC_Start(m_channels[i].p_handle) == HAL_OK );
        ASSERT( HAL_ADC_PollForConversion(m_channels[i].p_handle, 10) == HAL_OK );
        ASSERT( HAL_ADC_Stop(m_channels[i].p_handle) == HAL_OK );
        *(m_channels[i].p_last_raw) = HAL_ADC_GetValue(m_channels[i].p_handle);
    }

Any help appreciated.

Cheers,

Jorgen.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

When converting more than 1 channel, you need to use DMA to avoid an overflow in ADC->DR. What chip? I'm sure there's an example in a CubeMX repository.

If you feel a post has answered your question, please click "Accept as Solution".
Jorgen1
Associate II

We are using STM32H750.

There are examples on using DMA, but I didn't find anything showing or explaining what to do when all three converters are used.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.