STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

32F756G-EVAL2 : Demo Code provide

Dear STMicroelectronics.​Hi,I bought 32F756G-EVAL2 board.Lot code is Z0T10278E021.​Do you provide demo code?I didn't find it in the resource.​In the case of the compiled demo, it is a damaged file and contains only media file.I look forward to your r...

KCha.1 by Associate
  • 945 Views
  • 1 replies
  • 0 kudos

Keil MDK-ARM VS IAR EWARM VS CXSTM32 IDEs

Hi everyone,just got myself a STM32F0 Discovery kit as I wanted to try out a M0 chip, as I'm going to install the development toolchains, I found several of them that I could potentially used but not sure which one is more suitable for my needs. So ...

PWong by Associate
  • 6783 Views
  • 3 replies
  • 2 kudos

Qspi dummy cycles issur

We are working with stm32h743 and W25Q128JV We used to have 6 dummy cycles, but when USB is initialized we need to change it to 4.Than we tested another board and it was changed again to 2.Why? What is wrong

Problem with interrupt time to compare

Hello I have some problems with an interruption on the STM32H7. I'm working on a project and i implemented a timer with two interrupts (OVF and CC1) and that worked. But after trying to implement HSEM that no working even with an old version. That'...

OADDI.1 by Associate II
  • 714 Views
  • 0 replies
  • 0 kudos

STM32F072RbT6 I2C1 not working.

Hello,I am using STMCUBEMX 5.2.1 to initialize the configurations of my STM32F072RBT6. My application requires the use of i2c1 since i2c2 is already occupied on our board by a pressure sensor. However, it seems to me that i2c1 is not working (i.e. th...

YGehl.1 by Associate II
  • 2353 Views
  • 5 replies
  • 0 kudos

Hi i am using stm32f746zg nucleo board and i want to establish communication between two CAN modules where CAN1 should transmit and CAN2 should receive the msg but its not happening dont know why ..can anyone help me with the code ..?

here is my codevoid can(void){   CAN_TxHeaderTypeDef TxHeader;   uint32_t TxMailbox;   uint8_t usr_msg[10]={'h','e','l','l','o'};      TxHeader.DLC=2;      TxHeader.RTR= CAN_RTR_DATA ;      TxHeader.IDE= CAN_ID_STD;      TxHeader.StdId= 0x65;   if(HA...

B Vinod by Associate II
  • 4831 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.