STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am trying to use ISM43362 WiFi module in B-L475E-IOT01A1 target as a server. I am unable to get client connection details when I start more than 3 servers or restart a server on a port for more than 3 times

Please find the goals and the issues belowGoal - Start server on 4 sockets one by one, then keep on looking for a client for all the four sockets. When a client is connected to any of the server, I want that server to start sending/receiving the data...

PMaha.1 by Associate II
  • 847 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F303 - SPI1/DMA1 ch2 receiving only one byte

Hi all,I have trouble with receiving one byte on SPI1-DMA1. All is working if I set more bytes to transmit/receive (2 and more) but when I try to send only one byte it do not trigger interrupt on Rx channel (DMA1 channel 2).I can see transmitted byte...

is there a way to implement SPI burst mode in stm32f401?

Hi All, I am trying to use STM32F401 NUCLEO Board to talk to ST IMU LSD6DSL. LSM6DSL supports burst mode read, but I can not find a way to implement SPI burst mode from the stmf401 s library. I am wonderinf if there is any way to implement a SPI bur...

jb by Associate II
  • 2550 Views
  • 4 replies
  • 0 kudos

Stop2Mode wake up, i2c don't work

Hi,I am using stm32l431 and work with LPTIM in stop2mode. When the mcu wake up after stop mode, i2c stop working, so I need to restart mcu.It's strange because in some cases the i2c work in the next 3 wake up, but after this dont work anymore. Should...

GFont.1 by Associate III
  • 1381 Views
  • 1 replies
  • 0 kudos

Resolved! Power configuration issues

Hello everyone,I've just realized a PCB using STM32H7A3 micro. But at second step I already fell.I've my system powered up at 3.3V from an external circuit. The quality seems to be good.I've tried to program the micro using STlink through a SWD port....

MNico.2 by Associate II
  • 1365 Views
  • 1 replies
  • 0 kudos

uart interrupt repeat

Hello friendsI'm communicating with uart.finishing operations on interrupt and while going backbut does not go back to interruptmy codeswhile (1) { /* USER CODE END WHILE */   /* USER CODE BEGIN 3 */ for(int i=0; i<7; i++) { rx_buffe...

Iatik.1 by Associate II
  • 1004 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.