STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4xx I2C slave not working

I'm currently trying to setup a STM32F4DISCOVERY Board with the STM32F407VGT6 chip as a I2C slave. Somehow the controller doesn't send any ACK bit after the address was received. I've tried with the General Call function as well.Here is my initialisa...

MBind.1 by Associate
  • 1201 Views
  • 1 replies
  • 1 kudos

nucleo-g431kb voltage reference buffer

Hello everyone!I'm want to use the internal reference voltage buffer of the mcu stm32g431kb as input with comparator, but when i checked the reference manual they say VEREFBUF must kept disabled because no VREF+ pin in 32 pin package!!I don't want th...

0693W000003Bte5QAC.png
LLah.1 by Associate II
  • 1179 Views
  • 1 replies
  • 0 kudos

stm32f103 spi communication with ad7730 random wrong number

I am communicating with ad7730 (24bit adc) using atm32f103ZCT6. I try to read one of the registers of the adc but each time I receive a random wrong figure. The strange thing is that while debugging using serial wire (STLINK) everything is perfect an...

DKari.1 by Associate II
  • 2081 Views
  • 3 replies
  • 0 kudos

How do I configure MCU as an I2C slave device?

Remark : I am asking this question again, since even after trying multiple times on my own, and asking on other platforms, nobody has answered it yet. I can't figure out how am I supposed to configure as slave. So sorry for that. I am not able to del...

KSchr.11 by Associate II
  • 2091 Views
  • 2 replies
  • 0 kudos

What "EXTI" stands for ?

Hi AllAbout EXTI :In some stm reference manual about "EXTI" i read some strange things : For example:In STM32f070 Ref. manual "EXTI" stands for " Extended Interrupt/event Controller".In STM32f407 Ref. manual "EXTI" stands for " External Interrupt/eve...

Syous.1 by Associate
  • 6892 Views
  • 7 replies
  • 1 kudos

I2C communication with multiple slaves

Hi guys may I ask for your inputs on the I2C communication. I am using STM32F103C8 MCU with 2 slaves on the I2C bus. 1st slave is PCF8574 IO expander and 2nd slave is MCP4725 DAC. I'm using CubeMX to generate my codes. What I wanted to do is use ...

RSy.1 by Associate III
  • 5555 Views
  • 5 replies
  • 0 kudos

SPI non-DMA max speed ?

I am communicating with a TFT LCD and trying to speed things a little bit. At the moment I dont have DMA library written, so I am using standard SPI mode.I configured the SPI clock as 5Mhz on STM32F407 mcu. My main clock is PLL on 96Mhz. With APB2 = ...

0693W000003BpLnQAK.png
Gossamer by Associate II
  • 6832 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.