STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! After erasing internal flash using st link utility when i will start storing sum data into internal flash it is going to be in hard-fault.

Hello Everyone,We are working on STM32F413RH. We are storing sum data into internal flash at some interval of time. Simple mechanism is used, first we are erasing sector and then we are writing our data into internal flash.But when we are erasing chi...

MGami.1 by Associate III
  • 1808 Views
  • 7 replies
  • 0 kudos

Where are timer outputs connected?

For instance STM32H750VBT6 has many timers, but CubeMx does not show where their outputs would go. I don't want to mess (enable all of them) an existing design just to see where timer output are.

LMI2 by Lead
  • 1894 Views
  • 6 replies
  • 0 kudos

Resolved! Is there a problem with STM32F098CC Datasheet ?

In STM32F098CC/RC/VC pin definitionsit is saying that PB4 has USART5_RX for LQFP48 but when i looked at PB4 AF's in Table 13. Alternate functions selected through GPIOA_AFR registers for port A , there is not USART5_RXand AF4 is empty(even there is n...

YAY.1 by Senior
  • 2338 Views
  • 4 replies
  • 0 kudos

DAC OUTPUT

Hi againI'm using STMG071 with 2*DAC. I need them as negative inputs to COMPx.in order to use PA4/PA5 for other purposes – I set  DAC1->MCR      =0x00030003; so DAC will not be output to the pin (PA4/PA5).Yet – as soon as DACs are enabled (DAC1->CR 0...

YWhit by Associate III
  • 1072 Views
  • 1 replies
  • 0 kudos

Slave SPI Receive Only Interrupt

HiI have (had) a working project with an EXT interrupt which was wired to the CS pin of a SPI bus.Although it was working I had various bugs, particularly a timer interrupt, which TDK helped me resolve earlier.I've had great success with SPI master, ...

Smoun.1 by Associate III
  • 709 Views
  • 0 replies
  • 0 kudos

Nucleo F334R8 - basic example of a Timer TIM2 mystery

Hi guysSo I am developing a small PWM generator around the F334R8, it's overall extremely simple. All the work is done with another MCU sending data on SPI.On the F334R8, an EXT interrupt is called when the CS line is pulled down. From there the F3 l...

Smoun.1 by Associate III
  • 4829 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.