STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about STM32H743 Errata Sheet ES0392 Rev 7

In Section 2.2.13 of ES0392, it states that there is "unexpected leakage current" if Vin >Vdd.What is the bound on the leakage current (assume an FT pin type):Vin = 5V and Vdd = 1.8VVin = 5V and Vdd = 3.3VVin = 3.3V and Vdd = 1.8VThank you.

losing some isr

Hello dear experts,I am using the TIMER2 on stm32F446Re with TI1_ED as reset mode input and TIM2_CH4 as timer value capture input. I inserted code to toggle a gpio in the HAL_TIM_IC_callback. On the scope I am capturating the TIM2_IC4 signal and the ...

papageno by Associate III
  • 1415 Views
  • 2 replies
  • 0 kudos

ADC DMA with TIM21 TRGO conversion source on STM32L010

I've got an application where I'm performing an ADC DMA transfer where the ADC conversions are triggered by the TIM2 TRGO. Everything was running smoothly until a PCB respin forced me to switch over to TIM21 to trigger the conversion. I didn't see a ...

DWann by Associate III
  • 5779 Views
  • 12 replies
  • 0 kudos

Storing small data in internal flash

HI, we are working on STM32H750. in our program, we need to store 5 bytes in the internal flash. this data will be read everytime the device is powered on. the data will be changed whenever the settings are changed by the user. i.e. once in a while.M...

dv.13 by Associate II
  • 1414 Views
  • 1 replies
  • 0 kudos

RTC backup date and time

Hi,I created this function in order to store the date and time. It works !But the problem is when I load date and time, the time is the last before turning off the system.void RTC_Init(void) { /* Restore the date form backup registers */ RTC_LoadDa...

MMerc.1 by Senior
  • 2641 Views
  • 4 replies
  • 0 kudos

Resolved! using PWM with STM32L412

I have PWM setup on my STM32L412, but there is no output on the pins. I move a value to CCR1, CCR2, CCR3 but there is no output. I'm using cubeIDE to generate the HAL setup, but I notice that the timers aren't enabled, but this isn't the solution - e...

deep_rune by Associate III
  • 1662 Views
  • 3 replies
  • 0 kudos

Resolved! Why HSE is not getting ready?

Hi guys,I am using an stm32L552ZE with an NX2016SA-24MHZ-EXS00A-CS10820 oscilattor. Everithing runs as expected until i get to HSERDY waiting. I get a timeout at this part. For startup I am not running a cutom code and the HSE on code is:SET_BIT(RCC-...

CDan.1 by Associate II
  • 2953 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.