Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi,I wanted to Erase and write data to select Flash memory location.I have Nucleo-L4R5ZI kit and have example Flash erase code available for L4 series which I ported to R5ZI.As you can see, the example code has two portions:Erases the page(s) which w...
In the STM32G4 reference manual, section 30.8.15 has TIM16 and TIM17 OR1 at address offset 0x50. This register is used to enable the HSE/32 input to TIM16/17 for measuring the frequency of the HSE clock. In section 30.8.22, the register map summary...
Hi, I am using stm32l432kc nucleo and BMP280 sensor with I2c communication.During the debugging I realized that the data from the sensor is not updating, always 2481 (temp32 variable).Could you help me in this topic?Thank you in advance.Info:Used dri...
I am trying to use CAN on STM32743ZI eval board. . I am able to transmit and receive data in loopback mode successfully without any error but in normal mode I am getting transmit errors. The FDCAN interrupt registers are 0x31800000. It means that pr...
Dear community,I am programming an ST32F407VE for the first time (I don't use the Cube32IDE though). First, I made an on board LED blink, so I am pretty certain that my toolchain and framework work properly. In the next step, I wanted to implement a ...
Hi,I'm using a STM32G030 controller and I'm working with ADC Timer-triggered and DMA for storing the data. I need a quad-buffered DMA that generates an interrupt when 1/4 of the buffer has been filled. I'm not experienced with this so I'm asking some...
Hello, I'm trying to debug an custom board with STM32L010C6 and STLINK V2. The firmware download seems to work fine, but the debugging is not working. The execution stops here:0x1FF00220 4800 LDR r0,[pc,#0] ; @0x1FF00224I've already tried to brea...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.