2020-09-06 5:23 AM
I would like to know if the SPSRF could work for us?
can it pass UART/SPI/CAN/etc. side to side?
thanks
2020-09-06 11:20 AM
That's really not how these devices work, if you need to tunnel data over the radio link for other hw protocols you have running, you'll have to implement those methods.
2020-09-07 1:12 AM
Hi Clive,
from the SPEC the of SPSGRF its support SPI, is it transfer SPI over the radio link? point to point?
if not, what data is it transfer over the wireless link, can i build it that it will transfer the SPI packet and rebulid it on the RX side?
thanks,
2020-09-07 6:37 AM
Hi there in Amimon -v))
Clive is right, this is not how it works.
To pass thru SPI or UART, you need to know the data layer protocol and wrap the protocol messages to transport over wireless,
then unwrap on the other side and forward. Think how to compensate for added latency and loss of messages over the wireless.
On the other hand, if you had a broadband wireless link such as in your wireless video, it could accommodate a few MHz subchannel to carry UART, maybe even SPI.
-- pa
2020-09-09 2:09 AM
hi Pavel,
thanks,
we going to buy the 2 EVB boards of B-L475E-IOT01A1, in order to bring-up a demo of network between 2 EVBs, base on subGHz RF.
do you think it is good platform for quick start POC subGHz network link?
maybe, do you recommended on other EVB platform for POC?
i mean platform with reference code for bring up the network and send first packet side to side.
thanks a lot,
Meron
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.