2020-09-08 5:38 AM
Hello dear experts,
I am using the TIMER2 on stm32F446Re with TI1_ED as reset mode input and TIM2_CH4 as timer value capture input. I inserted code to toggle a gpio in the HAL_TIM_IC_callback. On the scope I am capturating the TIM2_IC4 signal and the ISR (callback) generated toggled signal. Between two TI1_ED event , I should have around 100 IC captured signal but I can see that not all input signals produce an ISR. Looks like I am missing some ISR. The reset mode input is a video frequency (let's say 24fps) and the capture TIM2_IC4 (channel4) is 2.4Khz. I dont understand why I am losing some ISR ? What could explain that behavior ? 2400hz is not such a high frequency. The ISR checks the timer and the channel number and send a 32bits on the uart using DMA. All the involved timings do not appear so difficult to process especially for a 90Mhz timer and proc.
Any suggestion for anybody ? Weakness of the signal (needs pull-ups ?? ), level of priority and preemption for signal ?
Thanks in advance.
Pap
2020-09-08 6:57 AM
Interrupts get delayed by running interrupts of equal priority, oar arriving interrupts of higher priority.
Cube is (in-)famous for busy-waits and convoluted interrupt code. Especially check callbacks, they are executed in interrupt context.
Consider rasing the priority of the timer interrupt.
> I dont understand why I am losing some ISR ? What could explain that behavior ? 2400hz is not such a high frequency. The ISR checks the timer and the channel number and send a 32bits on the uart using DMA. All the involved timings do not appear so difficult to process especially for a 90Mhz timer and proc.
You could do a simple verification. Apply a known number of input pulses, and count them in the handler.
If your troubles are caused by coincidental interrupt overlapping, you might need a larger number of test pulses.
And, as usual, with toggling different GPIO lines in differernt interrupts, you could visualize the timing behavior, using a scope or logic analyzer.
2020-09-09 6:16 AM
thanks Ozone,
I tried all the things you proposed but i still miss some IRQ . I put a gpio low and up in the root of the TIM IRQ (TIM2_IRQHandler) to try to bypass the HAL extra code but I do not even enter that ISR.... very strange. i still miss 10ù of the IRQ. I also ried to put the TIM2 to a highest sub priority but it is the same. It s very amazing... the most disturbing is that I do not understand why I miss those irq. From the scope the IC signal looks good (11µs negative pulse level 3.3v at 2.4Khz).
i will dig a little more that problem, tickling my curiosity now.
Paps
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.