STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F746NG DISCO DMA Quad-SPI flash memory example.

I believe the QSPI Flash memory is in the memory mapped mode on the DISCO board. I programmed a 2KB bin file into the flash memory using the ST Link utility. I want to read this to internal ram. I set this project up with CubeMX. Can I change the fla...

Resolved! CAN setup on STM32F303

I've been working with CAN on the STM32F1 for some time , but I'm having a terrible time trying to get it to work on the F303. I'm hoping someone can tell me what I'm doing wrong. Thanks very much for looking at it.void can_gpio_config(void) { GP...

Resolved! Why voltage drops while using GPIO as a timer input

Greetings.I've entirely stuck with this problem.MCU: STM32F407VGT6Realization: custom PCB and F4 Discovery board.Problem: Microcontroller can't gather information from encoders.Description:   There are three motors with built-in encoders that I want ...

PWM Timer generation not working with low duty cycle

At low duty cycle (like below 5%), the timer pwm stops periodically (see the attached picture). The higher the duty cycle, the smaller the stop period. Does anyone know why this happens?For context, I am using the STM32F072 Discovery board. I use Cub...

0693W000003RBXMQA4.jpg
vtran1 by Associate II
  • 3000 Views
  • 5 replies
  • 0 kudos

I am using STM32F4 processor. The problem I am seeing is that at times the processor resets and the CSR register reports 04 in reset cause which is NRST pin reset. Problem is that we do not see any reset on the NRST Pin.

Scope is configured correctly. Reading of CSR register is done way early in the code and is reliable. Register is cleared after reading. Scope is configured correctly.When we trigger pin reset externally, we can catch it on the scope. When we trigge...

RBharol by Associate III
  • 3579 Views
  • 4 replies
  • 0 kudos

Examples of using the HAL libraries for using I2C as both master and slave on a single I2C interface, i.e. in a multi-master configuration?

Hi there,I'm trying to implement a multi-master I2C network, where there are several nodes (around 6), any of which can send a message to any other. In other words, all nodes usually acting as slaves, waiting for incoming I2C messages. When any node ...

JElso by Associate II
  • 4544 Views
  • 4 replies
  • 0 kudos

Resolved! Interfacing code of Ws2812b on stm32F1 is working but in a same way when i am trying it with Stm32F4 it is not working !!!!

TIM_HandleTypeDef htim3;DMA_HandleTypeDef hdma_tim3_ch2;/* TIM3 init function */void MX_TIM3_Init(void){ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; htim3.Instance ...

Resolved! I have a question about the STM32H743...

If this device is powered-down (i..e voltage is 0 on all rails), what impedance will be presented by the Port pins? If a pin from a powered-down STM32H743 is connected to a pin on another (fully powered) device, what current drain will occur?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.