STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

special incremental encoder reading

There is a very old machine that I want to remake.I cannot change the machine's sensors. The incremental encoder of one of the motors produces a jitter-like signal below at position 0. How can I determine this in reading with a timer. I am using STM3...

0693W0000059s90QAA.png

Resolved! Flash Sector Erase - STM32F207

Hello, I currently have this code setup to erase a specific sector of the STM32F207 internal flash:static void eraseSector(uint32_t sector) { FLASH_EraseInitTypeDef eraseInitStruct = { 0 }; HAL_StatusTypeDef status = HAL_OK;   if( HAL_FLA...

Anvi by Associate III
  • 2432 Views
  • 3 replies
  • 1 kudos

STM32F7 and Extern SDRAM Bank Accessing Problem

Hi everyone,I'm using a STM32F769BGT6 with an external SDRAM (IS42S32400F). This SDRAM is composed of 4 banks. Each bank contains 12 Rows (4096), 8 Columns (256), and each cell is 32 bits. So : 4096*256*32 = 33 554 432 bits, or 4MBytes/Bank. That mea...

STM32407x ADC , DMA and overrun

Hello, I want to know when ADC DMA is enabled and if ADC overrun status sets to 1. the RM says this >>>>>>>>>>>>>>>>.To recover the ADC from OVR state when the DMA is used, follow the steps below: 1. Reinitialize the DMA (adjust destination address ...

n.serina by Associate III
  • 1661 Views
  • 1 replies
  • 0 kudos

High start up time for STM32L4

I'm currently developing a project that will see a high number of MCUs connected in the end application so low power consumption is critical. I was aware there will be some initial high power consumption when first powered up however the MCU takes ~3...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.