2020-10-29 11:58 PM
Hello,
I want to know when ADC DMA is enabled and if ADC overrun status sets to 1.
the RM says this
>>>>>>>>>>>>>>>>.
To recover the ADC from OVR state when the DMA is used, follow the steps below:
1. Reinitialize the DMA (adjust destination address and NDTR counter)
2. Clear the ADC OVR bit in ADC_SR register
3. Trigger the ADC to start the conversion.
>>>>>>>
Question 1 ) with what value NDTR needs to be adjusted ?
question 2) when i trigger the ADC(step 3 above) will the sequence start from the beginning or will it resume from the channel where data was lost due to overrun ?
Thank you very much
2020-10-30 6:46 AM
When this happens, clear the flag and treat it as an entirely new conversion. I would be very surprised if it has any memory of where it was in the process. You could use the current NDTR value to determine where it left off.
Despite this, if data are lost (overrun), the OVR bit in the ADC_SR register is set and an
interrupt is generated (if the OVRIE enable bit is set). DMA transfers are then disabled and
DMA requests are no longer accepted. In this case, if a DMA request is made, the regular
conversion in progress is aborted and further regular triggers are ignored. It is then
necessary to clear the OVR flag and the DMAEN bit in the used DMA stream, and to reinitialize
both the DMA and the ADC to have the wanted converted channel data transferred
to the right memory location.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.