2020-11-26 12:56 AM
hey,
i have an STM32L432KBU6 and i want to serial communicate with my chip. I connected the SWCLK, SWDIO and the SWO pin and followed a couple tutorial on youtube but i just cant get the Serial communication done. i just want to open serial monitor like the adruino has. i tried it with the VCP(virtual com port), cuz my st link v3 has it and it doenst work.
sorry for my bad english, but if you have the answer i would be very happy :)
thanks for reading it.
2020-11-26 3:42 AM
SWO pin is different than VCP. Both do work, e.g. on a STM32L432 Nucleo32 board. Board schematics are avail for reference. You may also consult app note "stm32 microcontroller debug toolbox"
hth
KnarfB
edit: SWO is avail on the newest Nucleo-32 only (G431KB) and larger Nucleo boards
2020-11-26 4:57 AM
You'd need to wire a UART to use the ST-LINK/V3 VCP
To use SWO you'd need to use your debugger, there is a Serial Debug in Keil, and the ST-LINK Utilities and STM32 Cube Programmer should have a SWV Window. Need to have the core clock right for it to work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.