2020-11-26 7:18 AM
The reference manual (link below) gives some details regarding setting the high and low voltage thresholds for the ADC's analog watchdog in the ADC_HTR and ADC_LTR registers. However, I can't find any details explaining how the values put into bits [11:0] in each register map to a voltage. I assume that setting all 12 bits in ADC_HTR would equate to the highest possible threshold voltage, but how do we know what that voltage is? And does setting all bits in ADC_LTR mean that the low threshold is as low as it can go? Or does clearing all 12 bits set it to the minimum?
Happy Thanksgiving!
Here's a link to the reference manual:
Solved! Go to Solution.
2020-11-26 8:35 AM
The ADC within the STM32 always refers to the voltage between VREF+ and VREF-, which are connected to VDD and GND in your NUCLEO.
While the setting of all bits corresponds exactly to this voltage (0xFFF / 0xFFF * Vdiff) and clearing them to zero (0x000 / 0xFFF * Vdiff).
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-11-26 8:35 AM
The ADC within the STM32 always refers to the voltage between VREF+ and VREF-, which are connected to VDD and GND in your NUCLEO.
While the setting of all bits corresponds exactly to this voltage (0xFFF / 0xFFF * Vdiff) and clearing them to zero (0x000 / 0xFFF * Vdiff).
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-11-26 8:41 AM
Thank you! And I assume Vdiff = VREF+ - VREF-?
2020-11-26 9:48 AM
Yes, absolutely correct.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.