STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is a 32GB MicroSD HC 1 still a micro SD HC for stm32F446RE ?

Dear experts,My SanDisk Extreme 32GB V30 MicroSD HC 1 is not recognized by HAL.... SDIO 4 bits .Stay stuck in the SD_Init...Is that SD card not compatible with the standard implemented in HAL and the MCU ? Time is short and I cannot dig in the lower...

papageno by Associate III
  • 4285 Views
  • 6 replies
  • 1 kudos

About the output specifications of NUCLEO-L010RB

Hello.I am using NUCLEO-L010RB.What I want to do is to monitor the trigger with the GPIO pin during stanby mode, the sequence operation of the GPIO pin at the time of triggering, and the output of 16MHz from the MCO.However, in the current configurat...

ANaka.1 by Associate
  • 1588 Views
  • 2 replies
  • 0 kudos

STM32F446ZE spread spectrum clock generation

Hello,I am looking at the documentation for spread spectrum clock generation and I can't see how or where it should be implemented.Any help or pointing towards the documentation that will explain it would be appreciated.Thanks

Ckerl.2 by Associate II
  • 1997 Views
  • 2 replies
  • 0 kudos

Running STM32H745 at 480 MHz and using WFI

Hello,In RM0399 Rev 3, way down in the SYSCFG section 13.3.10 describing SYSCFG_PWRCR, we have the following note at the end of the register description:"Note: VOS0 must be activated only in VOS1 mode. It must be disabled by software before entering ...

CAN-BUS line goes bus off state at high temperature(70C°)

I have a CAN-BUS line communicating at 50kb/s speed. There are only 2 products communicating with each other on the CAN-BUS line. One of these products has the STM32L496RGT MCU (the clock speed of the CAN module (APB1) is 80Mhz.) and the other one ha...

0693W000005CBiIQAW.png 0693W000005CBi3QAG.png
aliozkan by Associate II
  • 2942 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.