STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i am trying to read two timers frequency count and store in DMA , here i have configured two timers in TIM2_CH1, TIM5_CH2 in the input capture direct mode. i used HAL_TIM_IC_Start_DMA() functions to get frequency into DMA , Am in correct a approach ?

i am trying to read two timers frequency count and store in DMA , here i have configured two timers in TIM2_CH1, TIM5_CH2 in the input capture direct mode. i used HAL_TIM_IC_Start_DMA() functions to get frequency into DMA . is it correct approach .i...

NPULI.1 by Associate II
  • 1096 Views
  • 0 replies
  • 0 kudos

Resolved! Output Pin

Hi, I have a Nucleo 144 - STM32H743ZI2 and I need that the output pins deliver 5V, no 3.3V. Is it possible?Thanks

SRivi.1 by Associate II
  • 2008 Views
  • 3 replies
  • 0 kudos

CAN TD does not reach VCC on STM32F412CGU6

I am using a STM32F412CGU6 and selected PB_9 to be the CAN Tx pin. The pin then idles at 2.8 volts. If I use it as a standard IO pin, it will go to 3.3 volts. If I assign the CAN Tx pin to PA_12 it also idles at 3.3 volts.I am using mbed 5.12

Avan .7 by Associate
  • 1689 Views
  • 3 replies
  • 0 kudos

Need flash organization for stm32f429bit6

According to the ordering information, this device provides 2MB of flash.But table 6 on page 77 of the reference manual that shows flash organization for stm32f42xxx devices shows only 1MB of flash, although it says "2 MByte" in the heading. This see...

JWolf.4 by Associate
  • 1384 Views
  • 3 replies
  • 0 kudos

Resolved! TSC Channel selection

Hello Everyone!I have thoroughly understood touch sense controller peripheral of STM32F051C8T6, I have also developed a test code using the HAL layer and is working file and detecting touch (i.e. is count value decreasing when finger comes near elect...

Resolved! Can an MCU that supports QSPI use OCTOSPI memories?

I want to add some volatile memory to my MCU (32~64 MB). I'm currently looking at STM32H/F7 devices.Most DRAM needs so many traces that the PCB area taken up by the memory makes it impractical for my design.It seems like there is a new memory interfa...

STM32H750 + QuadSPI PSRAM chip: would it work?

I wonder if STM32H750 will work with QuadSPI PSRAM chip (for example ESP-PSRAM64H) and map it into the memory natively? I've read in the datasheet that MCU supports Flash chips via QuadSPI, but what about PSRAM?

sminder by Associate II
  • 1958 Views
  • 1 replies
  • 0 kudos

How do the driver files from the firmware link to a program?

Can anyone help me with connecting the drivers that are missing in the example program I am trying to build for the audio recorder?I have tried everything I can think of and the program won’t link the header files. I am have tried to add the header f...

0693W000006El97QAC.jpg
SWall.2 by Associate II
  • 3031 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.