STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 spurious reset (RCC_FLAG_PINRST)

Hi, I have a project using STM32F407 micro. Every few days I get a reset on the device even though there is no interaction with the device. I have it running on the debugger with ST-Link connected and when this reset occurs I inspect the CSR register...

joe by Associate III
  • 3539 Views
  • 4 replies
  • 0 kudos

Why does HAL_RCC_OscConfig() fail on demo code?

NUCLEO-F429ZImxcube v6.1HAL_RCC_OscConfig() fails using demo project I believe it fails exactly here:pll_config = RCC->PLLCFGR;                                           if((READ_BIT(pll_config, RCC_PLLCFGR_PLLSRC) != RCC_OscInitStruct->PLL.PLLSource...

YPear.1 by Associate II
  • 2563 Views
  • 6 replies
  • 0 kudos

When using BG431B-ESC1 to erase the flash chip, IfI encountered that "unrecognized uC", "it is locked " What should I do? st-link util v4.1 usb drv v5.0.2 cli v3.1 fw V2.J34.M25 upgrade V2.J28.M18

When using BG431B-ESC1 to erase the flash chip, IfI encountered that "unrecognized uC", "it is locked "What should I do? Stlink version details, at below.Why upgrade # is smaller?st-link util v4.1usb drv v5.0.2cli v3.1fw V2.J34.M25upgrade V2.J28.M18

ktoke.1 by Associate
  • 1344 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F042K6 Nucleo CAN bus receive issue

I am trying to test the CAN bus on STM32F042K6 Nucleo board. I can transmit data but cannot receive. Here is my settings. Data is sent from STM32H7 -Disco board whose CAN0 bitrate is set to 250K. I can send and receive data to/from STM32H7 board. So ...

hsamurai by Associate II
  • 2516 Views
  • 3 replies
  • 0 kudos

Coocox to Makefile causes ASM compiling error

I'm attempting to migrate an old project from Coocox, to a good old Makefile, and somehow, even though all the gcc options are the same, and I use the same exact toolchain, I get his error, following this command:arm-none-eabi-gcc -c -g -O0 -Wall $(...

TGeof.2 by Associate II
  • 1578 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo-H743ZI2 schematic not available

Hello,while Nucleo-H743ZI product page and schematics are available, I am unable to locate any for the Nucleo-H743ZI2 board. Could you please assist? Thank you!

DZovk.1 by Associate
  • 1390 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.