STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Checking ADC sampling time calculations for STM32407VG?

Hello,I was following a course and the section I'm at is using the ADC. They said the sampling time is 10us, but I calculated it to be around 2.3us.Taken from the datasheet:13.5 Channel-wise programmable sampling timeThe ADC samples the input voltage...

JSamu.2 by Associate II
  • 3703 Views
  • 3 replies
  • 0 kudos

Does STM32L431 support bit band operation

What are the SRAM bit band area address and its bit band alias area address, and the peripheral bit band area address and its bit band alias area address, if supported?

HSX.1 by Associate II
  • 5699 Views
  • 14 replies
  • 0 kudos

Debugging JTAG daisy chain

Hello, I have a 4 identical microcontrollers daisy chain wich seems to work...exept I detect 8 devices?... My setup is the folowing...I have a segger J-link edu mini and 4 wire JTAG. basically I dont got JTRST but NRST connected to the J-link... In t...

0693W000006F127QAC.jpg
LBeau.1 by Associate III
  • 4112 Views
  • 6 replies
  • 0 kudos

Real time data logging with STM32F446RE possible?

Hi guys,I am currently trying to get a real time data logging device up and running. To measure a voltage with ADC I am using the STM32F446RE that is capable of 12bit 2.4Msps or even 7.2 Msps in 3ADC interleafed mode. For my application I want as muc...

MStix.1 by Associate II
  • 5368 Views
  • 7 replies
  • 0 kudos

External Loader Failing on STM32h7b3i-disco Board

Application is generated using the CubeMX with TouchGFX generator. Works wonderfully... that is until I want to locate my assets in OSPI.Added this to the STM32H7B3LIHZQ_FLASH.ld file/* Memories definition */ MEMORY { DTCMRAM (xrw) : ORIGIN =...

0693W000006F4FOQA0.png 0693W000006F4FxQAK.png

How to parse raw stack data in hex (STM32F4)?

Hello,I'd like to ask is there any information about parsing raw stack data?I always save data from PSP stack when a HardFault happens. Here is an example:20020200: 00000000 0A461285 00000F7F 00000000 00000000 0812CA7D 0812CA9A 2002021020020220: <hex...

GFree.2 by Associate II
  • 4984 Views
  • 9 replies
  • 0 kudos

Resolved! Where to find the RCC Register and GPIO Register

Hi,I try to find the RCC and the GPIO register for the STM32l432KBU, but cant find it in the datasheet. i dont know if i'm looking wrong but i just cant find it. I need the Registers to enable the uart.Thanks for reading:grinning_face: !!bye,

OTosu.1 by Associate II
  • 1464 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.