2020-11-28 1:45 AM
Hello Everyone!
I have thoroughly understood touch sense controller peripheral of STM32F051C8T6, I have also developed a test code using the HAL layer and is working file and detecting touch (i.e. is count value decreasing when finger comes near electrode). I have also read the TSC section of reference manual several times. I am unable to understand how to change the channel of acquisition within a group.
Right now what is happening is that I have enabled all three pins of IO group 2 as input electrode and the final (4th) one has the SAMPLING CAPACITOR connect to it. But the aquisition process always aquire the first channel only.
I am NOT able to find any function in HAL lib to change channel NOR I am able to find any register that controls that.
Some where it is written that acquisition within a group is sequential, but it is NOT also happening, each time only channel 1 is acquired.
Solved! Go to Solution.
2020-12-08 2:34 AM
Hello Avinash,
Find 2 examples based on G4 TSC group acquisition.
1st example is based on HAL TSC.
2nd example is based on TSL (TouchSensingLibrary)
Regards. Olivier
2020-11-28 5:49 AM
2020-12-08 2:34 AM
2020-12-08 5:08 AM
Thank you all for your kind suggestions. I have finally figured it out! And my touch sensing app working great ! I will post details here if anyone else reading have the same doubts, then this would be beneficial to them.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.