STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

some question about DALI Slave in STM32F

DALI_RX port and DALI_TX port have been initiated twice in" void DALI_Init(TDLightControlCallback LightControlFunction) " and "init_DALI(OUT_DALI_PORT, OUT_DALI_PIN, INVERT_OUT_DALI, IN_DALI_PORT, IN_DALI_PIN, INVERT_IN_DALI, DALI_Interrupt, DALI_Err...

0693W000003P8hPQAS.png 0693W000003P8e6QAC.png
晓石.1 by Associate II
  • 1685 Views
  • 3 replies
  • 0 kudos

USART3,USART4 how to use

DearI use the STM32H7B3I-DK this board,and I read the manual.The instruction says I can use CN11 digital pin name D0 and D1,but D1 is (USART4_TX)​,D0 is (USART3_RX).Then how do I use the USART3, because do not find USART3_TX​

Khe.11 by Associate
  • 2743 Views
  • 3 replies
  • 0 kudos

I am using stm32h745 MCU for communication with external nVRAM using FMC example which is given in Repository. while writing to the memory chip select as well as OUTPUT Enable signals are coming as expected from MCU but i am not getting write Enable .

I am using stm32h745 MCU for communication with external nVRAM using FMC example which is given in Repository. while writing to the memory, chip select as well as OUTPUT Enable signals are coming as expected from MCU but i am not getting write Enable...

srikanth by Associate III
  • 1062 Views
  • 1 replies
  • 0 kudos

STMStudio GDB source code

Hello all from ST!The STMStudio ships a modified version of an open source software called GDB:As you see from the output above the GDB is licensed under the terms of GPLv3+.The GPLv3+ license require the modified sources to be shared.Could someone p...

0693W000006GPRcQAO.png

"STM32" vs "STM32 Arduino" - I2C difference

Hi, I am trying to debug my code with logic analyzer and see why my code works on "STM32 Arduino", but does not work on "STM32". Viewing at logic analyzer I see that "STM32 Arduino" much more consistent.Why could the message be different "0xD1 0x00" ...

0693W000006GOctQAG.png
JBond.1 by Senior II
  • 2760 Views
  • 5 replies
  • 0 kudos

Resolved! Practical DMA transfer speed from MEM to PER?

Hello community,I wrote program that use MEM to PER transfer, HALF WORD mode (16 bit). DMA transfers are clocked by TIM1. MCU is stm32f103c8t6 @ 72Mhz on "Blue Pill" board. As final result I got 16 bit sample values on PORTB at 360kHz speed. It see...

IIvan.12 by Associate II
  • 5331 Views
  • 4 replies
  • 1 kudos

RTC running fast on STM32L433

Hi I have setup the RTC on the STM32L433 and the clock is running about 5 second fast in 24 hours. I am using a 32.768KHz crystal, which is directly next to the processor . I have set the RTC->PREDIV_A to 0x 7f, and RTC->PREDIV_A to 0x ff, and selec...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.