2020-12-19 2:43 AM
Hello community,
I wrote program that use MEM to PER transfer, HALF WORD mode (16 bit). DMA transfers are clocked by TIM1. MCU is stm32f103c8t6 @ 72Mhz on "Blue Pill" board. As final result I got 16 bit sample values on PORTB at 360kHz speed. It seems too low . Theoretically I read that MCU can perform DMA transfers on about 40% of clock speed, which mean about 30MHz. What are DMA speed which you reached and where can be my mistake?
Solved! Go to Solution.
2020-12-19 12:54 PM
No, I mean the application note, https://www.st.com/resource/en/application_note/cd00160362-using-the-stm32f0-f1-f3-g0-lx-series-dma-controller-stmicroelectronics.pdf
It describes, how the DMA works, although unfortunately not in much detail.
Basically, it performs some arbitration (1-2 AHB clocks), reads on the source side (in your case SRAM, if there's no conflict on the bus with other busmaster e.g. processor, 1-2 AHB), then writes on the destination side (maybe 1-2 AHB clocks, then whatever sync happens in the AHB-APB bridge, then at least one APB clock - the 'F1 is the first STM32 and the only where GPIO are on APB). Very roughly, count 6-10 AHB clocks per transfer, i.e. say around 10M transfers per second. If you transfer successive ones and zeros, you'll see half the transfer rate as output frequency.
> May be the problem is that on "Blue Pill" probably is soldered counterfeit device or may be not?!
That, of course, is possible. Or, maybe these days, likely.
JW
2020-12-19 9:25 AM
> Theoretically I read that MCU can perform DMA transfers on about 40% of clock speed,
Where did you read that?
Read AN2548.
JW
2020-12-19 11:05 AM
Did you mean "Using the STM32F1x and STM32L1x DMA controller (AN2548)" - zip file with some example projects how to use DMA controller? If YES I not seen how it can help me:
So my question remain ..... what is PRACTICAL transfer speed which someone really obtained using SRAM->GPIO DMA transfer.
May be the problem is that on "Blue Pill" probably is soldered counterfeit device or may be not?!
How examples from AN2548 can help me to understand REAL DMA transfer speeds?!
Ivan
2020-12-19 12:54 PM
No, I mean the application note, https://www.st.com/resource/en/application_note/cd00160362-using-the-stm32f0-f1-f3-g0-lx-series-dma-controller-stmicroelectronics.pdf
It describes, how the DMA works, although unfortunately not in much detail.
Basically, it performs some arbitration (1-2 AHB clocks), reads on the source side (in your case SRAM, if there's no conflict on the bus with other busmaster e.g. processor, 1-2 AHB), then writes on the destination side (maybe 1-2 AHB clocks, then whatever sync happens in the AHB-APB bridge, then at least one APB clock - the 'F1 is the first STM32 and the only where GPIO are on APB). Very roughly, count 6-10 AHB clocks per transfer, i.e. say around 10M transfers per second. If you transfer successive ones and zeros, you'll see half the transfer rate as output frequency.
> May be the problem is that on "Blue Pill" probably is soldered counterfeit device or may be not?!
That, of course, is possible. Or, maybe these days, likely.
JW
2020-12-20 1:16 AM
Many big thanks JW,
pointed by you application note is enough detailed and helped me to understand real situation. So as practical report:
Kind Regards
Ivan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.