2018-12-15 8:27 AM
Hi
I have setup the RTC on the STM32L433 and the clock is running about 5 second fast in 24 hours. I am using a 32.768KHz crystal, which is directly next to the processor . I have set the
RTC->PREDIV_A to 0x 7f, and RTC->PREDIV_A to 0x ff, and selected the LSE clock, cant think what it can be, anyone help?
Thanks
Scott
2018-12-15 8:40 AM
Double check the measured frequency. Should be able to benchmark via a connected TIM, or if available on an MCO pin.
Check loading, check trim settings.
2018-12-15 9:16 AM
5 second in a day is about 60 ppm. Crystal tolerance is oftne 50 ppm plus some load capacitance mismatch and your number can be explained.
2018-12-15 9:37 AM
You can use TIM16
Example here for measuring LSI here, but can select LSE
STM32Cube_FW_L4_V1.13.0\Projects\NUCLEO-L432KC\Examples\RTC\RTC_LSI\Src\main.c
The math here is broken, destroys accuracy
/* Frequency computation */
uwLsiFreq = (uint32_t) SystemCoreClock / uwPeriodValue;
uwLsiFreq *= 8;
Use
uwLsiFreq = (SystemCoreClock * 8) / uwPeriodValue;
2018-12-16 1:26 AM
Use HAL_RTCEx_SetSmoothCalib to tune the frequency. Here is my clock set up. Note Prediv setting are different to allow sub second reading
The calibration value (Option.RTC_calibrate in my code) can be between -511 and + 512. n specifies the number of extra clock pulses to be "created" or "removed" every 2^20 real clock pulses. If my maths are correct therefore a change of +/-1 should equate to about 0.0824 seconds per day.
/* RTC init function */
static void myMX_RTC_Init(void)
{
int up=RTC_SMOOTHCALIB_PLUSPULSES_RESET;
int calibrate= -Option.RTC_Calibrate;
/* USER CODE BEGIN RTC_Init 0 */
/* USER CODE END RTC_Init 0 */
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
/* USER CODE BEGIN RTC_Init 1 */
/* USER CODE END RTC_Init 1 */
/**Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 7;
hrtc.Init.SynchPrediv = 4095;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
if (HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
if (HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
RtcGetTime();
if(sDate.Year<18){
/**Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 0x0;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
if(Option.RTC_Calibrate>0){
up=RTC_SMOOTHCALIB_PLUSPULSES_SET;
calibrate=512-Option.RTC_Calibrate;
}
HAL_RTCEx_SetSmoothCalib(&hrtc, RTC_SMOOTHCALIB_PERIOD_32SEC, up, calibrate);
}
2018-12-16 8:07 AM
Thanks Clive.
I will have to download the examples, do I have to install the latest cubemx , which wil instalkl the examples?
Scott
2018-12-16 8:09 AM
Thanks Peter
I will look into this. I am only using the 32.768KHz as the external crystal, what does it calibrate it against? Wouldnt it need a known frequency to calibrate against?
Scott
2018-12-16 9:26 AM
"Wouldnt it need a known frequency to calibrate against?"
The real world :)
"the clock is running about 5 second fast in 24 hours"
You would start with a value of -5/0.0824 = -61
this converts to
HAL_RTCEx_SetSmoothCalib(&hrtc, RTC_SMOOTHCALIB_PERIOD_32SEC, RTC_SMOOTHCALIB_PLUSPULSES_RESET, 61);I you were 5 seconds slow it would be
HAL_RTCEx_SetSmoothCalib(&hrtc, RTC_SMOOTHCALIB_PERIOD_32SEC, RTC_SMOOTHCALIB_PLUSPULSES_SET, 512-61);
2018-12-16 10:05 AM
Typically an HSE supplied source, or you measuring it via MCO pin output on a test fixture.
2018-12-16 10:06 AM
They should be in the repository if you have previously installed the L4 libraries. You can alternately pull the CubeL4 ZIP file an unpack and use that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.