STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743II : Timer Frequency Tolerance

Hello,I am working on creating a timer function using the timer peripheral of the STM32H743II, with a timer range from 1 second to 3600 seconds.I'd like to ask a question regarding the frequency accuracy of the timer.Let me first explain the current ...

keiju_0-1751263133451.png keiju_1-1751263178392.png
keiju by Associate
  • 719 Views
  • 1 replies
  • 1 kudos

RTC as wakeup-source on C0 family

Hello, I have found various guides on how to configure the RTC as wakeup-source. However, they do not seem to apply to the C0 family.In the CubeIDE I cannot find the depicted settings on RTC, (most notably, no option to select internal wakeup and con...

Panda by Associate III
  • 2871 Views
  • 10 replies
  • 4 kudos

Resolved! STM32L433RCT VDD12 pins - what should I do with them ?

I am using the NUCLEO-L433RC-P development board and in the process of designing my own PCB.But I am unsure what to do with the VDD12 pinsOn the NUCLEO-L433RC-P development board they are connected to an SMPS using an analogue switch.If I dont use an...

freeflyer_0-1751227979437.png

Missing section IRTIM in STM32U0 RM and more.

1. According to datasheet, STM32U0 family have an IRTIM (Infrared interface). But this section is missing in RM0503. Also in SYSCFG_CFGR1 there is missing IR_MOD and IR_POL bits.2. In RTC section Figure 297 it is missing RTC_OUT2 and RTC_REFIN pins. ...

AA1 by Senior III
  • 8354 Views
  • 18 replies
  • 4 kudos

FCLK Cortex clock of STM32F411CE microcontroller

Hello,STM32F411CE microcontroller.What is FCLK Cortex clock for the STM32F411CE microcontroller (see Figure 1 below from the STM32CubeMX (Clock Configuration tab))? Is this clock related to processor clocking? As far as I know, the processor is clock...

Mykola_Levun_0-1751116535486.png

Resolved! GPIO input at 12V

Good Morning, I want to use a GPIO input or a ADC input as a logical reader which gives 0 or 1 if it reads 0 or 12 Volts. However, I know the maximal rating is normally 3.6 volts for those pins. However, i saw that the Adc can still read 5 volts, it ...

Jad by Senior
  • 928 Views
  • 1 replies
  • 1 kudos

Resolved! STM32 Interleaved ADC Sample Timestamping

Hi, I am using STM32L476RG-Nucleo64 boards for one of my ultrasound projects. Basically, the process is:1)Send 2MHz pulses with pwm2) Sample 1000points with 8-bit interleaved ADC(500 each) and DMA3) Send ADC data through SPI.4) Wait TIM3 to trigger a...

Stm325 by Associate III
  • 1920 Views
  • 7 replies
  • 3 kudos

Resolved! 5 khz wake from stop mode

I have an application in which I'm required to check the status of an accelerometer 5000 times per second but it's a battery powered device so I want to minimize power consumption. I'm using an STM32L053C8 on a custom board with an external LSE cryst...

MMora.6 by Associate II
  • 1046 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.