STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to initialize FDCAN on STM32H753

[Request]I would like to know the correct procedure for initialization using the INIT bit of the FDCAN's CCCR register.[Situation]1) To reset the FIFO status, we are only performing the initialization start using the INIT bit of the FDCAN's CCCR regi...

USB on STM32H503

I'm having problems enabling USB on STM32H503.  This happens on both my custom board (STM32H503CBT6-based), as well as on MB1814B (STM32H503RBT6-based).  I observe no USB connection, no USB IRQ being invoked, no hardware handshake.  Here's the simple...

romp by Associate II
  • 1897 Views
  • 4 replies
  • 0 kudos

Resolved! GPDMA and hate about documentation

Hi guys, first of all, after many hours of study of this peripheral i have "few" points. I will try to be as nice and calm as actually possible.1: Does anyone in ST review documentation and code you are generating? RM0456 17.4.2 paragraph 2:"After en...

Eiffel by Senior
  • 2048 Views
  • 3 replies
  • 4 kudos

Problems when downloading STM32N6 projects

I just got my NUCLEO-N657X0-Q board, since i have never used a stm32n6 board before, i decided to start from the stm32cubemx. I started my project from ST board, and created a simple test program for MDK-ARM project.After I opened the project in the ...

OliverLyu_0-1751182971561.png OliverLyu_1-1751183153789.png OliverLyu_2-1751183257333.png

Resolved! STM32H747 with OV5460 low frame rate

I am using STM32H747 MCU with OV5460 camera. The FPS i got from the camera is around12-13 fps is that any method to increase the frame rate.I tried by increase PLL clock but there is no image received.Thanks

KHowe by Associate II
  • 1570 Views
  • 4 replies
  • 0 kudos

Resolved! DSI Host interrupt and status register 0 (DSI_ISR0)

Hello,We are currently using a STM32U5G9 with MIPI Port 2 lanes talking to ST7701S TFT driver. We found on power up when we have a lot of error in DSI_ISR0.PE3 and DSI_ISR0.PE4 are set, display do not start. Definition of this error is : This bit ind...

cr_qc by Associate II
  • 681 Views
  • 2 replies
  • 0 kudos

ULPI integration on stm32 mcu clock reference

Hi everyone,we are moving our design from usb full speed to usb high speed using STM32F76VI.We want to use the suggested module STULPI01A in order to achieve this.On datasheet is specified to use a precise reference clock.Since our application use a ...

Comp1 blanking not working inverted input

Hi,While working on the code for an STM32H7B0, I'm having issues with the blanking function of COMP1. Specifically, it works correctly when the comparator is in non-inverting mode, but if I invert the comparator's output (to detect falling thresholds...

garinus_0-1747737757678.png
garinus by Associate II
  • 910 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.