STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem with STM32F411CEUx and HAL on SDIO and ADC.

Hello everyone, first of all I apologize for my English as I am not fluent in it.I am using the STM32F411 and SE and when using two DMAs for Tx and Tx it always shows BUSY in HalState. This I have solved (although not totally yet) by choosing only on...

LLope.1 by Associate II
  • 1273 Views
  • 1 replies
  • 0 kudos

Nucleo STM32F091 skips startup script to 'LoopForever'

I've been attempting to debug a test application compiled for an stm32f091RC controller on its corresponding nucleo development board. To debug, I use st-util and arm-none-eabi-gdb. When I load the elf file through gdb, the stm correctly halts just a...

CBlus.1 by Associate
  • 745 Views
  • 0 replies
  • 0 kudos

Availability of STM32F303

Can we expect shortage issue to go away in the near future. Both JLCPCB and Digikey have been having stock issues for months. I'm unable to get the MCU I've designed my project around (F303C[B/C]Tx). Digikey only has the lower flash mem options avail...

DOCon.1 by Senior
  • 2546 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H743 FMC with ST7789 doesn't work without delay

I have an STM32H743 connected to a screen that uses ST7789 via FMC (i.e. parallel connection) using 8-bit bandwidth and A18 to select between command and data.The current code has an issue that the screen output is messed up (see pictures below) if I...

0693W000007Ev83QAC.jpg 0693W000007Ev8mQAC.jpg
UKatz.1 by Associate
  • 2161 Views
  • 1 replies
  • 0 kudos

On STM32h753 UART interrupt is working fine after programming the controller using keil but malfunctions after complete power reset ?

I am working on STM32H753 microcontroller. I want to receive string using UART interrupt and send the same string back on UART. The IDE is keil uvision 5. The problem I am facing is that when I first program the MCU UART is working fine and I am rece...

0693W000007EthkQAC.png
Akash_k by Associate III
  • 1711 Views
  • 2 replies
  • 0 kudos

About DFSDM filter configurations FOSR and IOSR

When I increase the value of FOSR and IOSR,Iam ​not getting the proper values output from the dfsdm filter it keeps varying and is not also proper HAL_DFSDM_FILTERREGULARSTARTDMA(&hdfsdm1_filter0) ​​H​ow to keep the values of FOSR and IOSR?

No STM32 Target Found - custom board

Hi guys, I'm starting from a bare STM32G070KB, and cannot for the life of me get it to connect.I had this problem with an STM32G071CB but was able to solve it. The problem I was having was that I couldn't get an ST-Link to read the chip on a breadboa...

UMoha.1 by Associate
  • 1026 Views
  • 1 replies
  • 0 kudos

STM32F050C4T6A I want to use as a drop in replacement since I cannot find stock in the STM32F030C8T6 When I installed it in my board I use two I2C ports and they both work but the manual says there is only 1 I2C port. Am I ok to use this chip?

STM32F050C4T6A I want to use as a drop in replacement since I cannot find stock in the STM32F030C8T6 When I installed it in my board I use two I2C ports and they both work but the manual says there is only 1 I2C port. Am I ok to use this chip going f...

RScam.1 by Associate
  • 1486 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.