STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Data from ADC (DMA) over UART (DMA)

Hi,I am trying to perform continuous ADC conversions from a microphone using DMA, save that data to a large buffer, and then transmit that data using Uart (DMA). I have successfully setup the ADC to perform the DMA conversions along with saving them...

kcire L. by Associate III
  • 4337 Views
  • 3 replies
  • 0 kudos

I2C Slave endless clock streching

Hi, I have the problem that I get an endless slave Clockstretching.STM32F072 I2C configured with CubeMX, Primary slave adress $32If I fire a Tx frame from a master with for example:HAL_I2C_Master_Transmit(&hi2c1, 0x64, buf, 1, HAL_MAX_DELAY);The cloc...

0693W000008Fz3wQAC.jpg
RNaas by Associate
  • 820 Views
  • 1 replies
  • 0 kudos

Resolved! Put interrupt in RAM or pre cache

Hello,I am using GCC and eclipse CDT. I need to execute an external interrupt very fast (every 4µs). There is not a lot to do in there but I use about 2.5µs of time in the interrupthandler. I tryied to put the handler in to ram wich gave me the reloc...

Standby current is sometimes to high STM32L151CBT6A

We switch several times the µC into Standby Mode and the current is as described in the specification.But sometimes over the Vdda Pin the current is 1mA. We switch adc/dac vrefint etc off. No BOR in use.We checked each Ports, but the current is comi...

ADC value not able to read.

Hi, i got a fan failure project . For that i need to select 2 adc channels in DMA mode for rms calculation , and 2 digital input for my powerfactor reading . here i am using AC (230Vac) and DC (5v) supply both .I select two timers with 100khz in...

Lchal.1 by Associate III
  • 2201 Views
  • 0 replies
  • 0 kudos

Is there a compile time conditional statement for debugging?

Hello everyone! I am trying to debug some code but there are some flags in flash that keep getting set when I exit debug and it enters run mode (or when I power up the sensor. Basically, anytime it gets a chance to run before I can get it in debug ...

JayDev by Senior II
  • 1332 Views
  • 2 replies
  • 0 kudos

Resolved! Use HSE on stm32g070kb

Hello everyone,I am trying to setup the clock of my STM32G070KB using a 8MHz external quartz. I tried 2 different ways, one from CUBEIDE, the other from libopencm3. I didn't succeed to make my application work yet. CUBEIDE : I see a warning near the ...

0693W000007EfYAQA0.png 0693W000007EfLBQA0.png
TKopp.67 by Associate II
  • 2968 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.