STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

My potentiometer in a adc led counter doesnt work

Im trying to do an ADC led counter, but when i debug my program i see the live expression and i can watch the changes in the potentiometer, but D10,D9,D8 AND D7 are on but with 1.8v, and d5,d4,d3,d2 turn on with 3.3v, the main idea is that when i rot...

ALope.6 by Associate
  • 1651 Views
  • 1 replies
  • 0 kudos

Resolved! Is sprintf() supposed to support uint64_t numbers?

This compiles with no warnings or errors: char buf[256];uint64_t bignum = 0x123456789;sprintf(buf,"bignum: 0x%016llx, %llu\r\n",bignum,bignum);HAL_UART_Transmit_DMA(&huart1,(uint8_t *)buf, strlen(buf));This comes out the terminal:bignum: 0x0000000000...

KiptonM by Lead
  • 2828 Views
  • 5 replies
  • 0 kudos

FMC and SDRAM sample

I'm using STM32F469 with 2M x 16 x 4banks (16MB) SDRAM.I'm just trying to run FMC_SDRAM sample for STM32469l-EVAL and it seems the first 256 data could write/read successfully.My question is that to access memories in 2 to 4 banks, do I need to send...

SYoko by Associate
  • 1288 Views
  • 1 replies
  • 0 kudos

STM32F7 and MPU

Hello everyone,I apply STM32F746BE with externel SDRAM 32MB (MT48LC16M16A2P-75 IT:D) and externel FLASH 16MB (MX25L12845GM2I-10G), Ethernet (LAN8710AI-EZK), LCD.Vector' table is located at 0x20000000. Firmware is runned from externel FLASH 0x90000000...

Anton1 by Associate II
  • 4848 Views
  • 10 replies
  • 1 kudos

Time consumption FFT calculation. CMSIS, STM32F401RE

Hello,i calculate an FFT with the STM32F401RE. It works fine so far. Here are the relevant code snippets:arm_rfft_q31(&S1, (q31_t*)fft_input_buf1, (q31_t*)fft_complex_buf1); //takes about 1760 µs   arm_cmplx_mag_q31((q31_t*)fft_complex_buf1, (q31_t*...

felix23 by Associate II
  • 4447 Views
  • 3 replies
  • 0 kudos

Can't set Option Byte with the attached function for the Micro STM32L151CBT6A Only when the controller is new from factory. If we erase and reset the option bytes the STM32 afterwards new flashing it works.

void init_OptionByte (void){    FLASH->SR |= FLASH_SR_WRPERR ;     // l�sche bestehende Fehler    FLASH->SR |= FLASH_SR_PGAERR ;     // l�sche bestehende Fehler    FLASH->SR |= FLASH_SR_SIZERR ;     // l�sche bestehende Fehler    FLASH->SR |= FLASH_S...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.