STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7A3: SPI not working if SCK disabled

I am trying to emit data on SPI MOSI without enabling the corresponding SCK pin. This is useful for instance to control WS2812-type LEDs.​However when I use `HAL_SPI_Transmit_IT` to transfer 3 words, the IRQ Handler gets called 3 times (triggered by ...

AGebr.2 by Associate
  • 2027 Views
  • 2 replies
  • 0 kudos

ADC lines behavior when STM32 is not powered?

Hi!I'm using an ADC line of the STM32 MCU to read battery voltage that goes from 6.7V to 8.4V.The battery voltage is given to the MCU via a divider (by 4, so the maximum voltage given to the ADC line of the MCU will be 2.1V).I wanted to know, if ther...

YGehl.1 by Associate II
  • 1127 Views
  • 1 replies
  • 0 kudos

Touch Key in STM32L1

Hello, We are currently working on touch sensing in STM32L1V8XA Microcontroller Below are the queries :1) How to get started with cap sense touch key in STM32L1V8XA Microcontroller. Do we need to use STMTouch touch-sensing library https://www.st.com/...

JArot.1 by Associate
  • 698 Views
  • 0 replies
  • 0 kudos

Hello, I am a novice, I want to use rs232 to communicate with the computer in stm32f072cb,I want to enter 123 and post 456。I use PA9, PA10 is TX, RX

/** ****************************************************************************** * @file 01_Transmitter/main.c * @author MCD Application Team * @version V1.2.0 * @date 19-June-2015 * @brief This code example shows how to confi...

Hjing.1 by Associate
  • 2563 Views
  • 5 replies
  • 0 kudos

Datasheat vs .stm32h745xx.h

I am trying to debug my USB and in the process I am going through all the registers defined in the datasheet vs stm32h745xx.h file and I see that in some cases the .h file has registers defined that is not in the datasheetGUSBCFG_CTXPKT : in .h but n...

LHoug.1 by Associate II
  • 924 Views
  • 1 replies
  • 0 kudos

Resolved! This specific CAN2 config crashes during HAL_CAN_Init(), why

Lets hope someone has a felicitously revelation, or a clue.I am using a custom board with a nice stm32f105rbtx, fed with external XTAL.Everything worked like a charm untill i configured the clock to be 72Mhz and readjusted the can parameters in CUBEM...

0693W000007ZNwVQAW.png 0693W000007ZNxsQAG.png 0693W000007ZNz5QAG.png 0693W000007ZO0DQAW.png
Javier1 by Principal
  • 1192 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.