STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How can I use Vdda/Vref pin to get better range for ADC

Hello. I need STM with external Vref 3V. But I don't need so much pins like 100pins in ST where we have special pin Vref. Could I use VDDA/Vref pin in STM32F103RC according to drawing belloow? I wanna connect precision voltage reference to VDDA on 3...

RGima.1 by Associate II
  • 8240 Views
  • 4 replies
  • 0 kudos

Resolved! LSE vs LSI for periodic wakeup from Stop

Does LSE have any power-saving advantages over LSI when the RTC is used to periodically wake up from low-power modes? Or does it just provide better accuracy for the RTC? For example, let's say you only use the RTC to wake up from stop mode, but neve...

DOCon.1 by Senior
  • 3878 Views
  • 2 replies
  • 0 kudos

STM32F103 timer interrupts with HAL_TIM_PWM_PulseFinishedCallback and HAL_TIM_PeriodElapsedCallback does not work as intended

I am trying to do a blink example for testing using built-in LED on bluepill. Unlike regular delay and period interrupts, i want to try a custom-duty blink, in which i want 3s on and 2s off, a total of 5s period.in main: HAL_TIM_Base_Start_IT(&htim1)...

MKanc.1 by Associate III
  • 1503 Views
  • 2 replies
  • 0 kudos

Resolved! Note about use of real name on this ST community forum

(edited this post from previous panic language; still think its good to keep it around - and a suggestion: there should be a tag/category for "Community Website")Well, since ST asked me to register for downloading software, I thought I'd be honest, a...

0693W00000AMpBnQAL.png 0693W00000AMpKBQA1.png
sdbbs by Associate II
  • 1567 Views
  • 2 replies
  • 0 kudos

Resolved! stm32f429 hardware iic

Hello!Hello everyone, recently there is a need to use stm32f429 hardware I2C as a slave, debugging a few days without normal communication, want to find a demo reference​thanks​

WDann.1 by Associate
  • 1188 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.