STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I have a ST-Link V3 with USB-C?

Dear STM-Community,It might be true that all of us have a micro-usb cable at home, but due to smartphones,tablets,... the way more convenient USB-C plug is the new standard on the market.Therefore I would like to start some upvope for a awesome USB-C...

LObki.1 by Associate
  • 1997 Views
  • 2 replies
  • 1 kudos

RTC resets on power-cycle despite battery

I've connected a CR2032 battery to the V_BAT pin on my custom STM32F746 board. Right now, the battery is connected directly without a Schottky diode. When I power the board off and on again, though, the RTC is reset to zero values.According to the ...

X-CORE-AI TFLite Micro runtime

Exist template for implement small neural network with TFLite Micro runtime (tensorflow middlewares) with Device application ??this example but for tensorflow runtimehttps://wiki.st.com/stm32mcu/wiki/How_to_perform_motion_sensing_on_STM32L4_IoTnode

Kuri by Associate II
  • 803 Views
  • 0 replies
  • 0 kudos

Update firmware through CAN on STMF103VG. Is this possible?

I see the option in cube programmer but it seems I need a ST-Link for this. Is it possible to program the micro over an established CAN network. Currently we use PCAN from peak systems.Just wondering how is the best way to update our application in t...

BB.1 by Associate
  • 1543 Views
  • 2 replies
  • 0 kudos

After relocating IVT using VTOR, application work only in DEBUG session but not without debugger or Programmer (flash Hex file)

Hello,I am using sample program RTOS Thread creation with LED toggling for STM32H723 nucleo board.LED toggles and application works properly with interrupt vector table at default Flash address 0x0800.0000. This works for debug session. This also wor...

VJAIN.1 by Associate
  • 11753 Views
  • 3 replies
  • 0 kudos

Modbus rtu on STM32L031G4

I want to implement the modbus rtu on the micro STM32L031G4 which library do you recommend?(if you use freeROTS how should I configure the micro da cube ide?)

Fscu.1 by Associate II
  • 5883 Views
  • 2 replies
  • 0 kudos

Set sdcard "temporary write protect" bit - STM32f7

Hi.I'm working on a project with a STM32F722 and a microSD card. I'm using HAL_SD & FatFS.I want to modify the CSD of the SD card to set the "temporary write protect" bit to 1, to protect the card from accidental writes.It is my understanding you can...

TGeof.2 by Associate II
  • 2245 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.