STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't find the X3 crystal recommended by ST from any supplier, nor can I find an equivalent that is in stock from any supplier.

Hi,I have a STMF32446ZE board and require an external crystal that isn't using the STLINK crystal. For x3 ST recommend the following: NX3225GD-8.000MEXS00A-CG04874The specs of this crystal are: Frequency Stability ±50ppm Frequency Tolerance ±20ppm ...

CLH by Associate II
  • 1228 Views
  • 1 replies
  • 0 kudos

printf on STM32H747 core M4 doesn't work

printf works on the STM32H747 M7 core once I add the following codeint _write(int file, char *ptr, int len) { int i =0; for ( i = 0 ; i < len; i++) { ITM_SendChar((*ptr++)); } return len; }and enable the "SWV" in the debug...

CHossack by Associate III
  • 1987 Views
  • 3 replies
  • 0 kudos

Does HAL_UART_Transmit() sends ASCII or binary?

Hi! Does anyone know if HAL_UART_Transmit() sends ASCII or binary? I've tried to send some data a serial plotter but nothing is being plotted. The format of the data sent follows the setting in STM32CubeMx. (It works on Arduino serial plotter)Serial ...

M7890.1 by Associate III
  • 6250 Views
  • 10 replies
  • 1 kudos

Resolved! I'm using SPI to communicate with a MIPI chip, the commands to the MIPI are sent as 9 bits but the data sent back is 8 bits.

I'm using SPI to communicate with a MIPI chip, the commands to the MIPI are sent as 9 bits but the data sent back is 8 bits. The 9 bit are set up in a uint16_t variable. Using HAL_SPI_Init the data size is set to 9 bits. When I receive the data using...

WScot.1 by Associate II
  • 3706 Views
  • 6 replies
  • 0 kudos

Which MCU support Capacitive Touch Button and Touch Slider

Hello support,I want to develop one product based on touch button and touch slider.so which STM MCU supports those features.and what are the softwares avaialble to develop firmware for touchand also i need hardware design guide for the same.thanks

MThak.1 by Associate
  • 1433 Views
  • 2 replies
  • 0 kudos

RTC with Internal Crystal - STM32F303CB

Hi,I am trying to use RTC with Internal Crystal, I am not able to initialize the internal crystal of RTC. I am trying to initialize the internal clock by the RCC_CSR_LSION flag but I am not getting the RCC_CSR_LSIRDY flag set by the controller.void R...

Connectiion error

​I am using STM32H743XI(we made board)However, an error occurred when connecting using the existing ST Link v2 product.An error occurred (No debug probe found connected to the USB port Session aborted)​​IAR 8.40.1 using ​The firmware(ST-Link) was als...

BPark.5 by Associate II
  • 1540 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.