2021-07-13 5:44 AM
Dear Sir,
I am Using STM32G030C6T6
How to transfer a File which has (.AMR) Format from UART1 to UART2 ??
2021-07-13 6:03 AM
Hello @Sn.17 ,
I am not sure I am understanding you, but did you mean that you want to to transfer a file (Asymmetric Multi-Rate encoded speech?) from a microcontroller to another using an UART?
Best regards,
@SBEN .2
2021-07-13 6:16 AM
Yes -(Asymmetric Multi-Rate encoded speech) Audio data.
Form One UART1 to Another UART2
2021-07-13 6:56 AM
Hello @Sn.17 ,
In this case, and in its most basic form, you can use the examples provided with the firmware package. This particular example seems to be a perfect fit for what you want to do : STM32CubeG0/Projects/NUCLEO-G031K8/Examples/UART/UART_TwoBoards_ComDMA.
Otherwise, please do consider that transmitting files (or encoded/formatted data in general) requires more than just sending the bytes and hoping that everything goes well.
Best regards,
@SBEN .2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.