Ask questions, find answers, and share insights on STM32 products and their technical features.
Hello Folks,I was doing my I2C example, and I realize that the STM board found an address with one left-shifted.I set my Arduino address as 70 -> 0x46 for hexadecimalvoid setup() { Wire.begin(0x46); // Wire communication begin }I connect my STM32F4...
3.7.5 Flash status register (FLASH_SR), Bit 3 PROGERR: Programming error talks about 0xffffffff and 0x00000000 while 8 byte entities are envolved (-1LL and 0LL)
Using an STM32H750 part, I've lived with the slack tolerance of the HSI until coming to the UART where a speed of 9000 bps is experienced from a configured 9600 bps. This is too far out to be of any use at all and therefore have decided to put on an ...
Hi!I'm using EA W162-XBLG OLED in SPI mode. Timing shown in datasheet is really weird. In instruction diagram there is 20 clock cycles, in data transmission 18. I try to get it to work with STM32F407VG, but I can only set 8 or 16 clock cycles. Maybe ...
I tried the STM32Cube Programmer but it could not connect to the board. I'm on Linux Manjaro. Many thanks
In dual ADC mode, the bit DMAEN is invalid as the doc said but in the below screenshot it is describing that the DMACFG bit in ADCx_CCR is effective only when DMAEN = 1.Please see the below snippets from the document. Need help from you whether I am...
We can read the data from ADCx_CDR register in dual mode. The upper half word of ADCx_CDR consists of slave data and the lower half word of ADCx_CDR consists of master data. But in the manual mentioned ADCx_CCR for master data and EOC cleared when we...
I have an STM32F7 Discovery card and I would like to know how to read a Wave sound backwards (reverse playback) via SAI and I2S interfaces ?I can play a Wave sound forward and change its speed with the library and documentation provided by ST.Thank y...
Hello,I am using the Nucleo-h745zi-q board.I want to know that is this board supports the nano framework?how can I get nanobooter and nanoclr files.Please guide as soon as possible.Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.