STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! how long an interrupt handler executes

i want to measure the time an interrupt handler costs.​1. set a specified pin low at the beginning of the interrupt handler and high at the end of the interrupt handler like this:void EXTI4_IRQHandler(void) { /* USER CODE BEGIN EXTI4_IRQn 0 */ HAL...

alun by Associate
  • 1160 Views
  • 1 replies
  • 0 kudos

PWM Pin Level

Hi All,I'm using stm32f1 series. & truestudio.I want to set the PWM pin "High" when pwm does't starting pwm.But when i initialize the pwm, pwm pin is "Low".How can i set the pwm pin "high" when initializing.

Glee.11 by Associate II
  • 2706 Views
  • 4 replies
  • 0 kudos

Porting ExtMem_Boot to STM32746G-Discovery

Hello Could someone please tell me if it's possible to port the ExtMem_Boot Template for the STM32F7508-DISCO to STM32746G-Discovery board ?Or did someone already port it and could share his code ?Thanks in advance Raphael

RStad.2 by Associate
  • 710 Views
  • 0 replies
  • 0 kudos

Resolved! Replace stm32f427vit6 with stm32f427zit6

Hi can i, if i change the lay-out of my board, replace the original stm32f427VIT6 with a ZIT6 without changing the code?Could get my hands on some ZIT6 instead of the almost unobtainable vit6 for free, but want to know if its possible without changin...

DSmit.111 by Associate II
  • 3352 Views
  • 4 replies
  • 0 kudos

Arm Assembly Timer İnterrupt

Hi everyoneI'm trying to write the timer interrupt code I wrote in C (pa3 pin blinks at 10 ms intervals) with arm assembly language, but it doesn't work.I don't know exactly how to do the timer interrupt in assembly language.I tried to write my own c...

Bicer by Associate II
  • 1081 Views
  • 0 replies
  • 0 kudos

Scanning multiple channels using polling on STM32f401Re

Dear ST community,I am using ADC to measure different voltages and I need a total of 15 channels and I need to measure ADC in a polling mechanism. When I useHAL_ADC_GetValue(&hadc1);It gives me value for only one ADC channel I am unable to receive va...

Maaz by Associate
  • 2130 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.