STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flashing large binary (> 1Mb) to STM32H753VIT not working

Hello everyone,For over a year I've been involved in a project using the STM32H753VIT microcontroller. The firmware has been in development for quite a while and has subsequently been growing.Currently, the compiled binary is at the point where it is...

0693W00000D1NukQAF.png 0693W00000D1NxZQAV.png
GtH by Associate
  • 5771 Views
  • 9 replies
  • 3 kudos

How to configure 32kHz LSE oscillator via HAL?

I think I've set up everything sensibly via STM32CubeMX to get HAL control of the LSE, but the external oscillator appears to be not operable. In particular, there is essentially no voltage on the 32kHz crystal pins, so of course it will not oscillat...

FMC for STM32 in muxed mode

Please help me with operation of the FMC module in STM32F407VE. It is necessary to connect external RAM memory; since FMC module in this microcontroller uses the address bus and data bus in muxed mode, its need to demultiplex this signals. For this p...

Kvon .1 by Associate
  • 2996 Views
  • 1 replies
  • 0 kudos

Resolved! ADC returns wrong value

I have a hardware that have on stm32g071 chip and mcp9700 temperature sensor. I tried reading temperature and i read 2040.(ADC 12bit resolution).I also measured directly on hardware using multimeter and i read about 0.7 V So ADC measures wrong. Addit...

oziesin by Associate III
  • 7574 Views
  • 12 replies
  • 0 kudos

Can the I2C2 block be used on STM32F107?

We're investigating replacing some STM32F105 processors with STM32F107 on a short time frame.The datasheet footnote says "SPI2/I2S2 and I2C2 are not available when the Ethernet is being used." Does that mean that I2C2 is never available or that you h...

STM32F446 I2C Registers OAR1 and OAR2

Are these registers two address of a I2C slave or OAR2 is a mask of OAR1?Mean:address slave = OAR1 AND OAR2. Ex. OAR1 = 0xE0 OAR2 = 0xF0. (OAR1 AND OAR2) are 8 address 0xE0,0xE2 .. 0XEE . Thank you Marco

MNoll.1 by Associate II
  • 1459 Views
  • 3 replies
  • 0 kudos

I2C Interrupts

Hello everyone!I would like to know what requirements are needed to work with sensors in a STM32 core F401RE using I2C Interrupts, and if that is possible.Thanks.I was searching in Internet but I don't find nothing.

JGóme.1 by Associate II
  • 3546 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.