2021-08-26 10:24 AM
Hi,
I am considering upgrade from STM32F4 series to STM32F7 or STM32H7(single core) series. However, the H7 embedded memory is not enough for the requirement. I would like to run simple RTOS scheduler. So there is need for external memory.
-QuadSPI interface - Flash(code and config storage)
I would like to interface the following through FMC
-PSRAM(program memory)
-SRAM(data memory)
-FPGA(memory mapped)
I have two questions.
Thanks
2021-08-26 11:03 AM
> What are the drawbacks of running code from external memory
It will be slower, and it's more complicated to load code onto external memory than the internal flash.
> Is it possible to interface(PSRAM,SRAM and FPGA to FMC)
PSRAM/SRAM yes. An FPGA can appear as anything, so yes, assuming you have compatible code on it. I would recommend doing a pinout in CubeMX to verify all pins are available.
2021-08-26 11:36 AM
Some reason you'd use SRAM/PSRAM over a large SDRAM?
You can have up to 256 MB of QuadSPI Flash allowing for execute-in-place. Can be banked to provide 8-bit.
eMMC on the SDMMC could provide for very large storage of data/code.
Watch out for having enough select pins, although you could divide down and decode a larger one externally.
2021-08-26 12:07 PM
@TDK Thanks. Agree. There would be lot of work in bootloader to load code from external flash to external RAM.
Reference manual says..."The FMC outputs a unique Chip Select signal, NE[4:1], per bank. All the other signals (addresses, data and control) are shared."
So using chip select, we can map
-PSRAM to FMC-NOR Flash/PSRAM Controller NE[1]
-SRAM to FMC-NOR Flash/PSRAM Controller NE[2]
-FPGA to FMC-NOR Flash/PSRAM Controller NE[3]
or
-PSRAM to FMC-NOR Flash/PSRAM Controller NE[1]
-SRAM to FMC-NOR Flash/PSRAM Controller NE[2]
-FPGA to FMC SDRAM Controller
@Community member Thanks. Seems i have to read application note about QuadSPI Flash XIP. Would it affect performance comparing to parallel interface?
2021-08-26 12:58 PM
Caching should mask the inherent/relative slowness of the SDRAM, or QSPI external memories.
Code could always be copied into a RAM.
In indirect mode the QSPI can address 4GB devices.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.