STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Example for Dual CAN filter bank configuration (using two CAN)

Is there any example for using CAN1 and CAN2 in a dual CAN MCU like the STM32F777, especially how to configure the filter bank using the ST HAL (cube) ??As I understand the filter bank is shared. Are the FIFO0 and FIFO1 also shared?Why is there a CAN...

JDeck.1 by Associate
  • 3666 Views
  • 1 replies
  • 0 kudos

Resolved! Clarification about connecting UART and SPI to the STMod+

I am trying to connect an SPI communication device and a UART communication device to my STM32H7B3I-DK using the STMod+. From the datasheet for the discovery board, SPI and UART use the same lines (pin numbers 3 and 4) to connect the connections on t...

0693W00000FCmnPQAT.png 0693W00000FCmnKQAT.png
JTurn.2 by Senior
  • 1893 Views
  • 3 replies
  • 0 kudos

STM32F7 SAI DMA FIFO error

When using DMA to realize a SAI transmit (double buffer, rearmed in HAL_SAI_TxCpltCallback), I found some very strange behavior.In some configurations, a FIFO error interrupt (FEIF, ref. manual p. 235) happens after a few seconds. The time until this...

STM32 Nucleo-F413ZH: Proper way to start a second PWM (delayed and internal trigger start [both trigger or gated] slaved mode) , on another timer.

General objective: Generate 2 PWM's on Timer 3 and Timer 4 respectively at 50% duty cycle, both with period of 2 seconds and phase shift of 1second between them (Timer4 will start 1 sec later).Because I want it to be precise, I am not considering usi...

0693W00000FCmCnQAL.png 0693W00000FCmDHQA1.png
EToh.1 by Associate II
  • 4227 Views
  • 6 replies
  • 0 kudos

double type calculation

Hello.At the next double type calculation,double a = 0.7; char b = 12; double c;   c = a * b;c is saved to 8.39999 in the register But 0.7*12 is 8.4How can I save 8.4 to the 'c' register?Thanks.

Kim.Andy by Associate III
  • 1225 Views
  • 2 replies
  • 0 kudos

Resolved! My STM32L051K8T6 gets stuck in an infinite loop in HAL_Delay(1000); but I know its a hardware problem, not a software problem. Where should I focus my hardware debugging on?

I have used this same chip on a previous project and managed to toggle an LED on and off using HAL_Delay(1000); function. I copied the same code across to my new project board, uploaded it successfully, toggled the LED on successfully but when I step...

0693W00000FCj26QAD.png 0693W00000FCj2GQAT.png
ARyan.4 by Associate II
  • 2574 Views
  • 5 replies
  • 0 kudos

Resolved! stm32f4 external interrupt problem

Hello,I'm using an stm32f411ce with an lsm6ds3 IMU and I want to trigger a read from the IMU with an EXTI. I've set it all in the code below and activated the interrupt on the IMU. the interrupt is set in PR register but handler is never called.Thank...

EPora.1 by Associate II
  • 4565 Views
  • 17 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.