STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Test stm32 pinouts to use in a force feedback project

Hello guys, so, Im trying to make a steering wheel based in a brushed dc motor and an encoder with a stm32f407vet6. So, I ordered stuff and started testing, the encoder was working until some time it just stopped out of nowhere and now it doesnt give...

RSant.4 by Associate
  • 1865 Views
  • 2 replies
  • 0 kudos

Resolved! Is it possible to use USART RX/TX legs to blink a led?

Hello!I have an STM32F411RE nucleoboard.I tried to use PA2 (TX) and PA3 (RX) as a general output. I enabled the clock access and also setted the mode register to general purpose output mode, but when I connect the LED and set the pin high nothing ha...

0693W00000GY0PrQAL.png
MSzal.1 by Associate II
  • 4419 Views
  • 9 replies
  • 0 kudos

Resolved! Send AT Command to GSM Module via UART

I am having a problem with this line. When i use sprintf to send command but in this command have "", so this line is error. I want to some advice and solution to this.Thanks

0693W00000GY0gTQAT.png
APhuc.1 by Associate II
  • 3172 Views
  • 4 replies
  • 0 kudos

STM32F469N - Cannot program option bytes, cannot erase flash.

I've got a custom board with an STM32F469, 32 Mbit of parallel flash, and 64 Mbit of external DRAM. This board had been working fine until an incident where execution or data fetch occurred on the external 32 MBit flash, which had not been programmed...

JVan .3 by Associate II
  • 1289 Views
  • 1 replies
  • 0 kudos

Create a custom cards using STM32L562

Hy,I would like to create a simple Custom cards using STM32L562.My first question is: Do you have a simple schematic with only essentials components ?And my second is:at the first initialisation, the MCU need a BOOTLOAD or particular manipulation (ha...

JCERE.1 by Associate
  • 2054 Views
  • 3 replies
  • 0 kudos

Resolved! how to set RTC alarm for all day in stm32f407vgt?

mcu: " STM32F407VGT Discovery Board - DICS1 "application: RTC ALARMi am trying to set the RTC alarm for every 15 minutes in all the day. in each RTCAlarmcallback function i am setting the RTC alarm again with sTime.Minutes + 15.if sTime.Minute...

Vinay1 by Associate II
  • 3643 Views
  • 6 replies
  • 0 kudos

Resolved! Unexpected Gain in OPAMP_PGA in G431

I am testing Examples/OPAMP/OPAMP_PGA/ in G4 package code, only to find the gain is not consistent as showed below:The OPAMP input values are 0.01,0.03, ..., 0.15, and gain is 16.However, I measured output at ADC side, the gain drops significant as i...

0693W00000GWAeJQAX.jpg
HDaji.1 by Senior
  • 7008 Views
  • 20 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.