STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F7 @ 192MHz: long data copy time?

Hello again,I recently checked the time the STM32F7 (192MHz) needs to copy one 32bit buffer to another one, and I'm a little shocked about how long that takes.(Maybe I expect too much, coming from 8bit µCs with 20MHz, an STM32 still feels like a raci...

LCE by Principal II
  • 3771 Views
  • 10 replies
  • 0 kudos

Resolved! STM32F767's ADC buggy?

I've been sampling some signals using this ADC, embedded in the board NUCLEO-F767ZI but when it reaches the 113th sample, samples are taken wrongly, as I have plotted the memory and the signal shown doesn't correspond the one I am generating. Find my...

SDomí.1 by Associate
  • 2115 Views
  • 4 replies
  • 0 kudos

Issue where flash memory range reads as all zero.

Hello, I’m working on a project using the stm32l562E-DK. The project is based on (mainline) TFM with a secure and nonsecure application, and bootloader. I’ve modified the TFM sector definitions to change the sizes of the sectors. The bootloader and s...

0693W000003RRFTQA4.png 0693W000003RRFJQA4.png
BBekk.1 by Associate II
  • 2771 Views
  • 3 replies
  • 1 kudos

STM32H7 SPI TXP flag not resetting

Hi EveryoneI have a very strange issue in the SPI of my STM32H745.Consider following information0) No Master present on the Bus1) SPI5 is configured in slave.2) No interrupts, no DMA just polling3) Following is the initialization code (FIFO is set to...

0693W00000GVnz9QAD.png
DGupt by Associate III
  • 3371 Views
  • 4 replies
  • 0 kudos

How to use scanf in stm 32 with dlib.

Iam using stm32 IAR workbench 8.20.Iam trying to run scanf. but scanf isn't reading first character of any data type. If enter 1234 through keyboard then it will print only 234.does anyone know how to resolve this issue???​

UKuma.4 by Associate
  • 809 Views
  • 0 replies
  • 0 kudos

ECC uncompressed X point Public key to Y point.

Hi Sir, we need to uncompress the ECC public key. Now we are using Crypto_v4.0.1 LIB. We could use it on comx_aead&hash&ecdh API. Please inform us how to use the ECC. We need the uncompressed X point Public key to Y point.

Jchu.1 by Associate
  • 1037 Views
  • 0 replies
  • 0 kudos

SWV ITM Data Console not working properly

Hello,I am working on Nucleo-h745ziq board. For debugging purpose required the printf function, I can't use the UART for that because its used for another working. So using SWI I am creating the printf function but it cannot print the all the othe...

0693W00000GXuhQQAT.png 0693W00000GXugnQAD.png
MDeva.1 by Associate II
  • 3120 Views
  • 1 replies
  • 1 kudos

STM32L476 Locks up during Radiated immunity EMC testing

I have a design with STM32L476 microprocessor that I am having EMC issues with. The processor is locking up at 100MHz to 240MHz radiated immunity EMC, 10V/m, and not recovering. Product Architecture is that there is an external 24V supplying power to...

0693W00000GXxHzQAL.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.