STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to wake up STM32L010 every 100ms?

I am new in st's mcu.I am going to switch my project to STM32L010 (Nucleo-L010RB).In my project, i need to let mcu going to stop mode and wake up it self every 100ms.How do i do it?Is there any code for me to study?

Flin.1 by Associate II
  • 1422 Views
  • 3 replies
  • 0 kudos

STM32L151: HAL ADC DMA wait for completion of transfer

Hello Guys, I want to read multiple channels from my adc using DMA.However I want to implement it the following way:while(1){1. Start ADC DMA (scan, discontinous conv.)2. Wait for the completion (the CPU should just wait until the conversion of the m...

Chrizzly by Associate III
  • 2061 Views
  • 2 replies
  • 0 kudos

Resolved! I am trying to display the time on a OLED display using the RTC and I can get it to work but I keep getting a warning. I know there is a better way and was hoping someone could enlighten me as to what I should be doing.

Hello I am very new to c programming and embedded design. I know there is a right way to do what I am trying to accomplish. I seem to be doing it the wrong way even though my code still "works" I am getting warnings on a couple lines of code. Line ...

JWire.1 by Associate III
  • 2302 Views
  • 2 replies
  • 1 kudos

Resolved! Why are my uarts not working after rcc clock configuration?

Hi all,I got a strange issue. I'd like to use USART3 or UART5 on my STM32F446 chip. We have the chip on a pcb, so I am not talking about the nucleo board. The issue is when I do the system_clock_config(), the listed uarts does not work. void init() ...

NGros by Associate III
  • 3325 Views
  • 5 replies
  • 0 kudos

Crack at the end of I2S tranmission via DMA on STM32L073

I'm running a STM32L073 to generate a sine wave tone via I2S in normal DMA mode. The amplifier is a MAX98357A. The MODE pin is connected to VDD so only left channel is considered. I2S runs at 48kHz and the uC clock source is internal. The output tone...

JSchu.5 by Associate II
  • 2055 Views
  • 1 replies
  • 0 kudos

How to reduce jitter in SPI (register mode)

Hi all, I am using register mode SPI for communication purposes, clock is 210Mhzinterrupt is for every 4khzinitialized SPI with HAL formatSPI data rate: 35MBpswhen I send data through SPI I can find some jitter inside it. But when I drive the same si...

Roshan by Associate III
  • 1849 Views
  • 4 replies
  • 0 kudos

Resolved! [STM32F412] SPI issue with MAX7219

I am trying to transmit through SPI to a MAX7219 chip on my STM32F412G-Discovery board. The system clock is running at 100 MHz. I am using a level shifter to handle the 3.3V -> 5V voltage changing. I have used this IC on an arduino so I do know it wo...

MB.2 by Associate III
  • 4660 Views
  • 8 replies
  • 1 kudos

Program data on flash from PC

Hi, I have a simple code running on STM32L0 MCUs. I will need to change some data on their firmware on each board depending on some analog properties of another component.There is a practical way to program a portion of memory with some data after th...

GMont.4 by Associate II
  • 2519 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.