STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM not working?

Hi.This is a really simple question but I don't seem to be able to figure out the problem. I was trying to generate a PWM output (using Timer 2 CH1) on my blue pill board but nothing appears on PA0 after I upload the code.Edit: I am referring to this...

M7890.1 by Associate III
  • 5020 Views
  • 4 replies
  • 0 kudos

Resolved! Count edge with TIM14 channel 1 ?

I use counting on TIM15 and now need change to 14 , but seems here external pulses counting dont work. FYI STM32F030Is any setup for 14 possible?

MM..1 by Chief III
  • 4956 Views
  • 13 replies
  • 0 kudos

Resolved! incorrect nand id stm32h7

Hi everyone First time i read the nand ID with fmc it was all good.It was 0x2c 0xF1 0x80 that the micron told.But some times it couldnt read the id and it was all 0xff.Now when i read the id, i get two different ids.first ox2c 0x1 0x2 0x3 and sometim...

DMA transmit/receive on lpuart1

I'm using the NUCLEO-H753ZI dev board and have been testing various tx/rx reception modes using HAL routines with RTOS for all the available uarts. I have them all working well except lpuart1. When I try to receive or transmit in DMA mode I get no in...

How to make Metal detector using STM32 MCU.

I want to make metal detector circuit using STM32 for material shorting specification of circuit is given below.It can detect ferrous and non ferrous both metal.digital out put hi when metal object detected.It can show detected piece area.It is capab...

Resolved! STM32L471 System Memory always mapped to 0x0000_0000?

Hi everyone!I have found that the System Memory (Boot ROM) is always mapped to 0x0000_0000 on the STM32L471RET6 that I'm developing on. The Flash Memory is mapped to 0x0800_0000 as expected but as soon as interrupts are triggered they jump to 0x1FFFF...

STM32G474RE NUCLEO board SIMD instruction test

HiI want to test the execution speed of SIMD instruction. My demo as below.16-bit addition, for example.I find the instruction __SADD16() in cmsis_gcc.h. The execution time using __SADD16 is 27us and the time without __SADD16 is 23us.  It seems like ...

0693W00000HnjelQAB.png
fhu.11 by Associate II
  • 3941 Views
  • 6 replies
  • 0 kudos

STM32H750VB HAL_RTC_GetTime() function returns to old value.

Hi, i'm working with RTC and having issue about getting time. I'm calling HAL_RTC_GetTime function with HAL_RTC_GetDate, it's return old value of time. For example time is 00:10:00 and i called gettime function, it's return 00:09:38. I'm getting time...

Eralp by Associate III
  • 7425 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.