STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L152RET6 bank 1 and bank 2 switching:

Good day,I need some advise with switching banks on the STM32L152.Here's what I currently do:Flash a new, blank MCU and boot from bank 1.BOOT0 is externally pulled LOW. BOOT1 is being used otherwise.Load firmware starting at address 0x08040000 (start...

0693W00000HnaBGQAZ.png
HMull.1 by Associate II
  • 1756 Views
  • 2 replies
  • 0 kudos

How to use IDB05A1 in low power mode

i am using IDB05A1 and STM32F401RE MCU, X-CUBE-BLE1. i am trying to use IDB05A1 in low power mode. When the data is available MCU wake up from low power mode.@Sebastien DENOUAL​ @Community member​ @Peter BENSCH​ @Andrei MENGHIA​ 

HAL_QSPI_COMMAND locks up the QSPI FLASH

Dear All,I'm using STM32H757I-EVAL board. My stm32 cube ide version is 1.7.0.I'm trying the basic operation of reading the manufacture ID of the QSPI Flash.Below is the initialization code, which I have configured using STM32CubeMX.static void MX_QUA...

Aarra.1 by Senior
  • 2922 Views
  • 6 replies
  • 0 kudos

FDCAN_Classic_Frame_Networking example

I am using the FDCAN_Classic_Frame_Networking example for the STM32G0 part. Instead of using the 64Mhz clock I have a 16Mhz oscillator connected. The example uses a 1Mb bit rate at 64Mhz. My hardware and ioc file are setup to use the 16Mhz as FDCAN1 ...

BMart.2 by Associate II
  • 831 Views
  • 0 replies
  • 0 kudos

Use one DMA channel with 2 different IPs ?

Hello.The project I am actually working on uses several peripherals such as USART ADC SPI etc. I am trying to use as much DMA as I can, but there is something that I miss in the reference manual and on the internet.Can I use ONE channel with TWO stre...

Aahai.1 by Associate
  • 1786 Views
  • 2 replies
  • 0 kudos

Firmware file for B-L475E-IOT01A_Iot_Node board

Hello,I was testing the B-L475E-IOT01A_Iot_Node board, and the inventek wifi firmware was written incorrectly, and the board crashed.Can I get a firmware file so I can rewrite the entire firmware for this board?

BSalt.1 by Associate III
  • 1542 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.