STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can stm32l4p5 use Word FLASH Program Type ?

Hello,According to my research, i cant find word flash program type for stm32l4p5 mcus. There are three diffrent types(DOUBLEWORD,FAST,FAST_AND_LAST). These types defined doubleword.Thank you for your help.

Eakyo.1 by Associate III
  • 1288 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H735 Multiplexed Memory Mapped OSPI Hyperram Hardfault

Hi, I use OCTOSPI1 and OCTOSPI2 in multiplexed mode to interface with two S27KL0641 ram in Memory Mapped mode.Those Rams are used for LTDC Frame Buffer and for other application data (structure, data ...).I started from the STM32Cube_FW_H7_V1.9.0\Dri...

JRand.1 by Associate
  • 3851 Views
  • 5 replies
  • 0 kudos

delay inside a EXTI9_5 callback function

I have been trying to create a asynchronous serial UART communication on GPIOA pin 9 and pin 8pin9- is RxPin8- is Txin order to sample the message at the right time I have create a dealy function using the DWT mechanism, the idea is to wait 1.5*(1/b...

FDCAN Arbitration lost / LEC error doesn't handled with IRQ in DAR mode. Probably - the potential hardware bug.

Hello guys.I try to catch the IRQ of arbitration lost and error code in LEC in FDCAN in DAR (disabled auto retransmission) mode.I have 3 devices in CAN network:   STM32F207 - 2 pcs   STM32H745Q (dev board) + external phy.All devices works good. They ...

SPI Tsize-Tser

Hello , ı read RM0433 ,I could not understand the process in the image below(page 2198)

0693W00000JNrN5QAL.png

Resolved! Nucleo L476RG - Turn on LED

I am using a NUCLEO-L476RG development board, I am learning to write GPIO drivers for STM32 family I am implementing a simple logic in which I need to turn on an LED when a push button is pressed.I have a strange issue: The Bread board LED turns ON w...

0693W00000JNq9WQAT.png
Tbone1 by Associate II
  • 5369 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.