STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FT5436 compatibility with FT5336 from STM32F746-DISCO

Hello,I have made a custom board based on the STM32F746. I am using a touch panel which uses the FT5436. My question is: are the FT5336 drivers provided by with the STM32F746 discovery board drivers compatible with the FT5436? I cannot make it work. ...

YTalh.1 by Associate II
  • 2888 Views
  • 5 replies
  • 1 kudos

Is this a correct code modification?

// stm32f1xx_hal_rtc.c line 827sTime->Seconds = (uint8_t)((counter_time % 3600U) % 60U);// to thissTime->Seconds = (uint8_t)(counter_time % 60U);

Imla by Associate
  • 2248 Views
  • 5 replies
  • 0 kudos

STM32H7 TCM RAM access speed

Reference manual says that TCM RAMs are accessible at the maximum clock speed without any latency, but to perform accesses at a CPU speed higher than 520 MHz, one must disable the ECC on this RAM through the CPUFREQ_BOOST option byte. What happens if...

MMn.2 by Associate
  • 3557 Views
  • 6 replies
  • 0 kudos

Resolved! I'm trying to create my own GPIO API using LL library on STM32F4. When declaring GPIO port I get warning: initialization of 'long unsigned int' from 'GPIO_TypeDef *' {aka 'struct <anonymous> *'} makes integer from pointer without a cast [-Wint-conversion]

Hey, I create some enums and struct to declare specific pin settings. In .h file I create these struct and enums:typedef enum { ePin_Led_Stat=0, ePin_Led_GPS_Fix, ePin_USART1_Tx, ePin_USART1_Rx, ePin_USART2_Tx, ePin_USART2_Rx,   ePin_Name_Last} ...

DSimp.1 by Associate III
  • 2844 Views
  • 2 replies
  • 0 kudos

How to get the ADC identifier when using DMA?

Hi!!I am using a STM32F4 Discovery board. I am using the ADC1 and ADC2, both with DMA. I need the conditional to know which ADC was the one that finished reading data. I tried if(hadc->Instance == ADC1) but it only works when DMA is not used.Could yo...

LSoll.1 by Associate II
  • 10120 Views
  • 13 replies
  • 0 kudos

A question about WiFi with STM32H7

Hello,I would like to use WiFi in a DIY project with STM32H743, in which I design hardware and software completely myself.I am therefore looking for a simple solution that is supported by the STM32Cube (middleware) on the software side and can be eas...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.