STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hard Fault after exiting Low Power Sleep Mode

Hi,I'm using a STM32L031. When I'm entering the low power sleep mode und an interrupt occurs i'm getting a hard fault. The programm counter from the stack frame has ether the value 0x00000000 or is pointing at the __ISB after the __WFI - depending on...

Brigei by Associate III
  • 1957 Views
  • 13 replies
  • 1 kudos

Receive high speed data from stm32 via com port

Hello. I am looking for an example or help, how i can receive data from stm32 at 100kHz with Python via com port ? ADC samples at around 100Khz and streams the data i am not sure how to receive it correctly at this high speed. Thanks  a lot 

LSamc.1 by Associate II
  • 1662 Views
  • 9 replies
  • 2 kudos

Resolved! Very bad performances on the stm32N657

Dear all,I am facing very poor performance with the STM32N657.I have some benchmarks that manipulate arrays of data in different ways.I ran these benchmarks onNucleo_H753 @ 480 MHz, with caches ONNucleo_N657 @ 600 MHz, with caches ONFor the STM32N657...

Clamping voltage still dangerous to my MCU?

Hi, I´m trying to implement ESD protection to a custom board, I found recommendations for this part number (USBLC6-2SC6), which clamping voltage is as follows Look at VCL Clamping Voltage  there are 12V and 17 V  Then the USB pins of my MCU accept a ...

Aldo_Flores_Aguayo_0-1755634258877.png Aldo_Flores_Aguayo_2-1755634816905.png

Resolved! STM32H7 consumes excessive current in custom board

Hi everyone!  I designed the board shown in the attached picture. It’s built around an STM32H745 microcontroller, along with crystal oscillators, a DAC, an EEPROM, and an NE555 that generates a reset signal when a button is pressed long enough.  Afte...

Screenshot from 2025-08-20 21-28-14.png RDT_20250820_1813023149851891707715935.jpg.png RDT_20250820_1813138112429209238513684.jpg.png
Rawcode by Associate
  • 1390 Views
  • 3 replies
  • 4 kudos

Resolved! FMC SDRAM design recommendations (STM32F446)

Hello,I am designing a board with a STM32F446 connected to an IS42S16160H SDRAM through the FMC interface.Could you please provide ST’s official recommendations regarding the use of series resistors on FMC lines?Typical values (22–33 Ω)?Any ST guidel...

Rihem_ by Associate
  • 711 Views
  • 1 replies
  • 0 kudos

Unable to initialize under USB_SH_HOST of H7R7

while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);The code failed to run, as referenced< https://community.st.com/t5/stm32-mcus/faq-troubleshooting-a-usb-core-soft-reset-stuck-on-an-stm32/ta-p/803224 >This article has been conf...

MECHO_0-1755171344097.png MECHO_1-1755171373282.png MECHO_2-1755171386029.png
MECHO by Associate III
  • 590 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.