STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I call STM HAL UART code in multiple files?

I have a file in my VisualGDB project that has all the HAL code necessary to talk to a GPS receiver through a UART. I can #include this GPS file in one of the other files in my project and the code in that file can talk to the GPS just fine. If I #...

magene by Senior II
  • 4555 Views
  • 6 replies
  • 0 kudos

Disable tracing on STM32H743

Hi Is it possible to disable the ETM on STM32H743?I know It possible to disable the tracing via trace pins or reading the trace data at low speeds using Jtag, but is it possible to disable the CPU from recording instructions into the ETM?Is that what...

deckhard by Associate III
  • 1692 Views
  • 2 replies
  • 0 kudos

Resolved! Bits sent out from SPI MOSI pin are received inversed by analyzer

Hi!I am learning to read the stm32f103c8t6 manual in order to be able to control the MCU without the HAL libraries. It seems that I have set up everything as it should be, but the result seems weird. If I write 0x00 to the SPI DR, I see 0x00 by the a...

0693W00000JPYTDQA5.png
GMan1 by Associate II
  • 3764 Views
  • 4 replies
  • 0 kudos

UART timeout in DMA Circular mode.

Hi, I have a question about UART + DMA.I have a sensor that needs to send data to my STM32. When the sensor is stimulated, for the duration of the event, it sends a byte approximately every 1 ms.To receive the data there are no problems, I used DMA a...

STM32H755 Rev. V RDP Error when erasing flash sectors

Hi there, Our application has a firmware update method that begins by erasing flash bank 2 sector by sector before writing the new firmware.RDP level is set to 0, but this shouldn't be an issue as we're only erasing a sector.Occasionally (Maybe 1 in ...

MJack.1 by Associate III
  • 6781 Views
  • 7 replies
  • 2 kudos

Weird LPUART interrupt behaviour

Hi,i write code in bare metal so every time i initialize a project in STM32CubeIDE i do it as an empty project. I made a project for STM32L011K4 and try to initialize the LPUART, in the startup file i can find that the handler for the LPUART1 name i...

XKeto.1 by Associate
  • 2318 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.