STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! WWDG - max timeout so short?

I'd like to use one of the watchdogs on STM32F407, but I'm surprised the maximum timeout of the WWDG is so short (around 50millisecs, depending on clock speed).This is very restrictive, for example a sector erase takes much longer than this (and is a...

s_ by Associate III
  • 4239 Views
  • 6 replies
  • 0 kudos

Is it possible to use UART with more than one buffer?

I have no idea why this code is not working. I am sending chunks of a file with UART followed by short instructions of 2 bytes to tell the MCU whether another chunk is coming or to start playing the file.The MCU receives the first chunk without an is...

EYako.1 by Associate III
  • 4810 Views
  • 9 replies
  • 0 kudos

Continously Receiving UART Data and Transferring to DMA without Generating Interrupts With Variable Length Data on the STM32L475RE

I am working on a portion of code that handles some UART messages that come in periodically from an LCD. The reception of a message over UART from this screen will generate a response based on the parsing of the message received.It is part of a large...

EGold.3 by Associate II
  • 6778 Views
  • 9 replies
  • 0 kudos

Resolved! Strange interrupt handler problem on STM32H7

Another day, another bug....I'm trying to use ADC3 with BDMA on H753. Started from some cube-generated code that assigned BDMA channel 0 to ADC3.Allocated memory in SRAM4. Added interrupt handler for BDMA_Channel0 and ADC3.When I start the ADC3, I hi...

Pavel A. by Super User
  • 5896 Views
  • 9 replies
  • 1 kudos

Is an STM32 compatible with TDM8 ? And if yes, with 2 streams of TDM8 in and 2 of TDM8 out ? Or is there any other solution ?

Hello, I'm quite new to STM32 (although I've been looking at it for more than a year) and I'd like to use it for a project that has been going on for somthing like 2 years now. It's a digital audio mixer especially designed for portable use for movie...

VCres.1 by Associate
  • 1234 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.